Hello,
I have designed the 4W amplifier according to the TI appnote for the TRF7960EVM and it is working well.
I have connected a 4X3in antenna to the EVM setting 1W of power output and was able to read the credit card size tag about 3 to 4 inches away from the antenna. As I increased the power (adjusting the pot of the LDO) I have noticed at one point increasing the distance between the tag and antenna no longer is able to read the tag.
Is this due to the fact that it doesn’t matter how much more power you apply to the antenna it’s how sensitive you are to read back that data from the tag. The only way to increase the reading range at this point is to increase the antenna size so that the reading is more sensitive to the tag data being sent back? Am I correct in saying this?
What would have a better reading range; having a bigger area & less turns antenna or smaller area with more turns antenna giving the same inductance value for both cases (1uH to 2uH)?
What the advantage between Parallel or Series resonance antenna? (with series resonance antenna can we get higher inductance value to match the 50ohms input)?
Thanks
Vlad