This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everybody
I got a pair of this CC2500 module (as in attached pic) to try out and made two separate RX/TX main modules. One of the mcu's is a 5V system with a level translator (TXB0104) to interface with the cc2500 module.
The transmitter module transmits a string of word values within a loop - simulating a data stream like this (see below):
My receiver MCU has an LCD attached to display received data but it shows only one iteration of slightly wrong values before stalling and after a few tries, now i dont receive any data at all.
I dont have the USB RF stick to debug so is there a method where I can query the hardware status internally to see if there is anything wrong with the hardware or any other advice/pointers you have about this ?
Thank you and regards
Soumitra
CODE:
const ADC_value : array[5] of word = (0x0064, 0x00FA, 0x01F4, 0x02EE, 0x03E8); begin while (1) do begin for loop := 0 to 4 do begin txBuffer[0] := 0; txBuffer[1] := Hi(ADC_value[loop]); txBuffer[2] := Lo(ADC_value[loop]); RfSendPacket(@txBuffer, 3); // send 3 bytes Delay_ms(2000); end; end; end;
Hi TA
Thank you for the reply and yes i did, in fact this is from a working example that was written for sending ADC values to a receiver.
Just in case these are the register settings used :
const cRFSettings : RF_SETTINGS = (
0x0A, // FSCTRL1 Frequency synthesizer control.
0x00, // FSCTRL0 Frequency synthesizer control.
0x5D, // FREQ2 Frequency control word, high byte.
0x93, // FREQ1 Frequency control word, middle byte.
0xB1, // FREQ0 Frequency control word, low byte.
0x2D, // MDMCFG4 Modem configuration.
0x3B, // MDMCFG3 Modem configuration.
0x73, // MDMCFG2 Modem configuration.
0x22, // MDMCFG1 Modem configuration.
0xF8, // MDMCFG0 Modem configuration.
0x00, // CHANNR Channel number.
0x01, // DEVIATN Modem deviation setting (when FSK modulation is enabled).
0xB6, // FREND1 Front end RX configuration.
0x10, // FREND0 Front end TX configuration.
0x18, // MCSM0 Main Radio Control State Machine configuration.
0x1D, // FOCCFG Frequency Offset Compensation Configuration.
0x1C, // BSCFG Bit synchronization Configuration.
0xC7, // AGCCTRL2 AGC control.
0x00, // AGCCTRL1 AGC control.
0xB0, // AGCCTRL0 AGC control.
0xEA, // FSCAL3 Frequency synthesizer calibration.
0x0A, // FSCAL2 Frequency synthesizer calibration.
0x00, // FSCAL1 Frequency synthesizer calibration.
0x11, // FSCAL0 Frequency synthesizer calibration.
0x59, // FSTEST Frequency synthesizer calibration.
0x88, // TEST2 Various test settings.
0x31, // TEST1 Various test settings.
0x0B, // TEST0 Various test settings.
0x07, // FIFOTHR RXFIFO and TXFIFO thresholds.
0x29, // IOCFG2 GDO2 output pin configuration.
0x06, // IOCFG0D GDO0 output pin configuration.
0x06, // PKTCTRL1 Packet automation control. //04
0x05, // PKTCTRL0 Packet automation control.
0x30, // ADDR Device address.
0xFF // PKTLEN Packet length.
);
Regards
Soumitra
What im getting from the GDO0 pin is 0x01 (RX FIFO: Asserts when RX FIFO is filled at or above the RX FIFO threshold or the end of packet is reached. De-asserts when the RX FIFO is empty.)
followed by 0x00
Also, the packetLength in the routine = 1, and I am transmitting a word value split into 2 bytes ... so i wonder if the packets received are correct or the modules are working fine themselves.
BOOL halRfReceivePacket(BYTE *rxBuffer, UINT8 *length) { BYTE status[2]; UINT8 packetLength; halSpiStrobe(CCxxx0_SRX); while (!GDO0_PIN); while (GDO0_PIN); if ((halSpiReadStatus(CCxxx0_RXBYTES) & BYTES_IN_RXFIFO)) { // Read length byte packetLength = halSpiReadReg(CCxxx0_RXFIFO);
Thanks and regards
Soumitra,
This indicates that you have not yet successfully communicated with the CC2500. The first step you need to complete is to be able to write and read to a register. Try various values except 0 and 255. Use an oscilloscope to debug the lines as you progress.
Regards,
/TA
Thank you TA
That was a great diagnosis.... it seems one of the SPI channels in my mcu is not working or initialized properly yet, due to a bad solder joint. Anyways, the SPI is working now and ive checked the data lines with the oscilloscope. But i still dont get the modules working.
Is there a way to check if the transmitter is working and transmitting the correct data ?
Thank you once again
Regards
Soumitra
Soumitra,
After you program all the registers, you now need to fill the FIFO with transmit data and issue "STX" command.
As a debugging trick, I typically poll the MARC_STATE registers as fast as the MCU will allow me to and store each result in an array for later analysis. Specifically what I do is read the MARC_STATE register 1000 times, then look at them to make sure the radio goes thru all the different states specified in the datasheet.
If the state of the radio ends up in a weird state, you can use this information to figure out what your next step is.
Regards,
/TA
Thank you TA
Just to confirm, the STX command is sent after a burst write within the HalRfSendPacket method. This is the same code as in the TI examples archive.
My mcu can be clocked upto 48mhz ... so I followed your advice and checked the MARC_STATE at different intervals in the code flow.
function GetMarcState: Byte; begin Result := HalSpiReadStatus(CCxxx0_MARCSTATE); end;
I get nothing from the status register before the
HalRfSendPacket(@txBuffer, 3); // send 3 bytes
But get a 0x00 (sleep) after sending the packets.
I also tried the following method within the lib but this does not seem to return any value as in the main execution block of the program hangs if i enable this debug method.
var RF_STATUS: array[255] of Byte; var RF_C: Byte; procedure GetMStatus; begin if RF_C < 255 then begin RF_STATUS[RF_C] := RfSpiReadStatus(CCxxx0_MARCSTATE); Inc(RF_C); end; end; procedure RfSendPacket(txBuffer : ^byte; size : byte); begin temp := RfSpiReadReg(CCxxx0_MCSM0); RfSpiWriteBurstReg(CCxxx0_TXFIFO, txBuffer, size); RfSpiStrobe(CCxxx0_STX); {$IFDEF DEBUG} GetMStatus; {$ENDIF} while(RF_GD0 = 0) do nop; while(RF_GDO = 1) do nop; end;
Im not sure what else I can do at this point. Any help ?
Thank you and regards
Soumitra