This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

When to use ASK, GFSK, 2-FSK, or MSK for CC1101?

Other Parts Discussed in Thread: CC1101

As I had understand, the ASK is for legacy products and it will be better to use frequency shift keying modulations.Does this mean that ASK doesn't have a place anymore for new product developments?

Also, assuming a scenario you have a data bit rate of 37kbps @ 433MHz, how do you determine which type of modulation will you use for a certain goal? Right now, I am doing just a short range communications, and GFSK, FSK and MSK all works well. But if I would pick one, which one should I use? And what are the factors I need to consider?

Also, the deviation given by SmartRF studio for FSK, is it already at it's optimal value? on which circumstances do we need to adjust that value?