This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

802.15.4 libreries for sub1GHz solutions

Other Parts Discussed in Thread: CC1200, TIMAC, CC1120, MSP-FET

Hi,

I'm comparing different 6LoWPAN solutions in both 2.4GHz and sub1GHz bands.

The idea is to compare the 802.15.4 physical and Mac layers first (link distance, capacity, etc)

I already made some tests with the cc2530 and cc2538 modules at 2.4GHz, but now I'm Using the CC1200 (TrxEB) and the CC1101 (SmartRF04EB), and I'm trying to validate the technology and compare with 2.4GHz.

The PERtest preprogrammed in the device is already using 802.15.4? If not, Can I test the 802.15.4 sub1GHz with another PERtest and the same device?

Are there any libraries and examples using 802.15.4 for sub1GHz applications for those boards? Like TiMAC for 2.4GHz.

Thanks