Hello
I just bought TRF7970A EVM Board and I downloaded and Installed Stollmann NFCStack+Eva TI R6.0.57.5
I also Installed USB Driver CP210x_VCP_Windows (WIN7 64Bit) for TRF7970A EVM.
I used TRF7970A_GUI_WIN7_11_2013 at first and it working properly, BUT when I want use Stollmann NFCStack+Eva TI R6.0.57.5 the "NFCPlayer" application can not connect to TRF7970A EVM.
My setting is "READERTYPE=NCI (TRF7970) IOTYPE=SERIAL PORT=COM12 " and also COM12 is set properly to use with USB.
- Please help me to know what is the problem and how I can use "NFCPlayer" from Stollmann NFCStack+Eva TI R6.0.57.5 software with TRF7970A EVM?
- Do TRF7970A support Read and Write DesFire EV1, MiFare cards in AES secure Mode?
Best Regards
Nader