Other Parts Discussed in Thread: CC8520
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC8520
Hi Lynn !
Looking at your scope grabs I see one thing I think is a bit strange :
Why is the SCK and CSN lines floating at about 1V before and after the CC debugger is trying to connect ?
Would seem to me that the 8520 is not getting the power it should.
From what I see in your schematic you should cut the line to pin number 9 on the JTAG connector and add IOVDD power to pin 2 of the same connector if it's not connected there now.
Ole A. Torvmark
Thank you for the input. Pin 2 is connected to IOVDD. We removed the RSTN connection to the CC8520 but all responses are exactly the same.
Hi Lynn!
First one comment: The CC8520 does not support broadcast, it will handle maximum 4 slaves in FW1.1 release....
Schematic looks fine....could you zoom in on MISO and MOSI, so I can see the comunication betwetween the CCdebugger and the CC8520?
Hi Lynn !
Have you checked the 48MHz crystal ? Is it running correctly ?
Ole A. Torvmark
Thank you for the help. We used a very small soldering iron and resoldered all the pins on the CC8520 and it now connects and programs.
Great! I'm glad you solved it, and thanks for sharing your solution on how you fixed it.