This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi. I am Minhyung.
I am going to use a RF430FRL152H and an MCU to build a custom device that will drive two LEDs and receive output through a Ligthsensor.
So first we put each chip on the PCB and then we made the test circuit on the breadboard. Antenna used RF430FRL152HEVM by separating it. As a result of operation, VDDSW: 1.5V, VDDH 2.1V works well. However, when I check the connection status with the GUI, I get an error message "could not read from device". What is the problem?
If the LED is connected, VDDH will drop to 1.8V. Is this related?
Dear Helfried,
Thank you for your reply. I solved the problem thanks to you. Your opinion is right. My chip was programmed, so I replaced the new chip.
However, when the VDDH pin was connected to the MCU, it still did not work. I checked the current of the LED. And it was pretty high. So I connected a resistor to the LED and it finally works fine.
I thought that too much current on the LED side would cause NFC communication to fail.
What do you think is the exact cause of this? I'm curious about your opinion.
Best regards,
Minhyung