Hello,
I am working on a design using the RF430. It is my first RFID project, and I am reading the practical guide to RF430 antenna design (SLOA217A). It is a very helpful document, but I'm unclear about the intended production process for tuning. The document kind of makes it sound like once the design is finished, a single external resonance capacitor value can be chosen to achieve the proper resonant frequency on all boards. However, section 4 of the document explains that the internal resonance capacitor is 35 pF ±10%. Given this wide range, it seems each board would need to be tested and then have a resonance capactor value selected in order to meet the -0/+1% resonance frequency tolerance recommended in section 5.4. Is this the expectation?
Thank you.
Tom Herron