Part Number: TRF7960A
Other Parts Discussed in Thread: TRF7970A, LM3S6965
Hello,
we are using TRF7960A since many years for ISO15693 transponder.
I try to implement the ISO1443A sequence in our project using your example sloc251.
Please find attached a dvdat file with the SPI communication between our microcontroler and TRF7960A.
There are 4 cycles recorded.
After the pollcmd I get TX and RX interrupt and can read the correct ATQA.
I get an answer to the anticollisioncmd. TX and RX interrupt and can read the first 3 UID bytes.
"88 88 88 16 38 04 A2" Byte 4-6 are the first 3 bytes of the UID, and the 7th byte is the checksum from byte 2-6.
(Transponder ID: 16:38:04:BD:90:7D:3D , ATQA: 0x41 , SAK: 0x20)
My problem is, that I do not get any answer from the sendselectcmd. No TX and RX interrupt.
Best regards,
Michael