This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Regarding Wi-SUN Stack Development

Part Number: CC1352P
Dear Sir,
 Can you please clarify the following points.
1)The concept of Border router with multiple node's network structure.
2)Is Non PA and PA (Added external power amplifier for better output power) software is compatible?
3)Provide the FOTA details and Time required to update FOTA (Stack as well as     Application)  using border router with multiple nodes.
4)Is border router source code will be provided to user development?
5)Available memory mapping for user application(After Wi-SUN stack usage),
    a)Program memory
    b)Flash
    c)RAM
6)Can we save the user parameters(like baudate,channel etc) in Flash as per user     requirement?
 
Regards,
Rajesh.M