This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The latest SDK versionsimplelink_cc13xx_cc26xx_sdk_7_10_00_98
a routine in CC1311, encountered the following warning when double clicking sysconfig to generate the driver configuration file, unable to run the command.
I have already configured the environment variables, as shown in the screenshot below:
thank you
Hi Alex,
I see that you are using IAR 8.32.1.
This SDK's release notes are stating that the minimal supported version of IAR for this SDK is 9.32.1.
Can you try with that version?
Regards,
Arthur
Hello, has there been an update on this issue? I have tried, but the same issue still reported an error
Hi Alex,
I have tried myself and it works. But I maybe see an error on your screenshots.
Indeed, it looks like your variables are pointing to the D: drive:
While SysConfig is trying to be launched from the C: drive.
Could you try copying the d:/ti/sysconfig_1.15.0 folder to c:/ti/sysconfig_1.15.0 ?
Regards,
Arthur