This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1311P3: CC1311P3 On-Chip debug enable

Part Number: CC1311P3


Tool/software:

We are trying to access CC1311P3 chip using code composer studio in the debug mode but we are getting "cant run target cpu error -2134". We are able to do debugging with launchpad with the same project source code,

Please let us know if we need to anything differently for the On-Chip device.

  • I am sorry, but I do not understand what you are asking.

    Have you made your own HW and are not able to debug/download code, while you can with the LP?

    What is the "On-Chip Device"?

    If you have made your own HW, what reference design have you used?

    Also specify which SDK version you are using, what example you are trying to debug, and which tools (and version you are using)

    Siri

  • Its our own HW and We have followed the CC1311 reference design (LAUNCHXL-CC1352P-4). We made a customization by removing the onboard MCU(MSP432E401YTPDT), its circuits and we have given CC1311 JTAG to header directly. Other circuits are same as reference.
    Tool Used: Code composer Studio v12
    SDK Version: simplelink_cc13xx_cc26xx_sdk_7_41_00_17

    We have enabled "Force VDDR" in the device configuration of the example project "uart2echo_LP_CC1311P3_freertos_gcc". With this setting, we were able to fix the above mentioned issue.
    Please help us understand how this could impact and also confirm if this configuration is expected.

  • Hi, Please let us know the impact of Force VDDR as mentioned in the above query.

    Also we are planning to use the following configurations with CC1311P3. Please let us know the RF configurable options available for the same.

    FEC: 1/2 rate convolutional coding

    Preamble (4 bytes): AAAAAAAA

    Sync Word (4 bytes): 91D391D3

    Whitening : Enabled as in CC1110

    Deviation: 3.707866 kHz

    Channel spacing: 363372.8027

    Manchester Encoding : Disabled

    Modulation: 2-FSK

    Center Frequency : 400.2 MHz and 450.1 MHz

    IF Frequency : 158.203 kHz

    Frequency Offset : 0

  • Hi,

    Changing the VDDR should not impact the debug capabilities. It could be that your VDDR is just on the limit of a threshold and forcing VDDR can be resolving this by increasing VDDR.

    Do you have any external circuitry connected to VDDR in your design ? 

  • Hi RGW,

    We don't have any external circuit, its connected to the IC DCDC, as per the reference schematic.

    Can you also please check and comment on the below configuration possibility in CC1311.

    FEC: 1/2 rate convolutional coding

    Preamble (4 bytes): AAAAAAAA

    Sync Word (4 bytes): 91D391D3

    Whitening : Enabled as in CC1110

    Deviation: 3.707866 kHz

    Channel spacing: 363372.8027

    Manchester Encoding : Disabled

    Modulation: 2-FSK

    Center Frequency : 400.2 MHz and 450.1 MHz

    IF Frequency : 158.203 kHz

    Frequency Offset : 0

    Thanks,

    Theiv

  • Hi,

    Can you please update on the above query, we are stuck currently.

    Thanks,

    Theiv

  • Hi Theiv,

    I saw that this thread has not been marked as resolved.

    Please can you create a new thread with your updated questions so I can follow this up for you?

    Regards,

    Zack