Other Parts Discussed in Thread: LP-CC1312R7, , CC1311P3, CC1352P7
Dear TI Team,
I would like to summarize the linked case to see if I understood everything correctly.
If I want to evaluate the CC1311 in a 434 MHz variant, I should use a EVK of the CC1312, use the BOM for 434 RF path from CC1352 and change the CC1312 to the CC1311 because it is pin compatible.
If this is correct, nevertheless I would have two questions:
- The CC1352 has more matching components. Are there enough pads on the CC1312 Eval Kit to fit this?
- Is the full setup in 0201 components?
Best regards
Tobias