Dear expert,
Could you pls check how to achieve 2Msps of CC1310? My customer want to achieve 2Msps but just 1Msps achieve.
I checked that a related question but the link couldn't open. could you pls check the information?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear expert,
Could you pls check how to achieve 2Msps of CC1310? My customer want to achieve 2Msps but just 1Msps achieve.
I checked that a related question but the link couldn't open. could you pls check the information?
The link opens at my side. Quote from the post "HSM mode on CC1310 refers to 4mbps fixed datarate with 8FSK modulation. It is possible to achieve 1mbps datarate 2(G)FSK and upt0 1.5mbps 4(g)FSK (programmable datarate) on this device as well in the 868/915MHz bands. Please refer to the following posts for settings needed for these modes."
Meaning that 2 Mbps is not an option.
Hi,
Thanks for your reply. The following link could not open. could you pls check?
The customer want to use 470~490M bands. Could CC1310 achieve 2mbps data rate at this band? Or should we suggest CC1311 or other device? Could you pls check the setting. The customer's project is pending and do you have any suggestion to solve the problem?
The achievable datarate is lower on the 433 MHz band than the 868 MHz band, the highest datarate on 433 MHz is 1.5 Mbps. This is due to the MIPs available in the RF core that is frequency dependent.
Some of the links for old E2E posts are corrupt but you can get them to work if you remove the last number (I don't know if they still point to the correct post though)
e2e.ti.com/.../cc1310-receive-nothing-using-433m-1mbps-with-rf_cmdproptxadv-rf_cmdproprxadv
Hi BU friend,
Do we have the test code for highest datarate 1.5 Mbps on 433 MHz?
Hi Chris,
We do not have test code for this set up Chris. The suggestion would be to find the settings by making use of the e2e threads that TheGhostOf linked and then use the generated settings on rfPacketTX and rfpacketRx.
Regards,
Sid
Hi Chris,
The answer by SVS in this thread seems to have the settings that TheGhostOf is referring to.
Regards,
Sid