This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: 868Mhz helix antenna modification

Part Number: CC1200


Hi.

I attach a proposition of a 868mhz antenna based on your DN038. As you can see my design is forced to modify the long feed track of the antenna because it is impossible for me to move the antenna feed point to the left.d

How much would it affect the antenna performance? Would still be possible to tune it with inductor/capacitors at the feed point? The original design has a distance of 6mm between antena tracks and ground but my design has a distance between antenna tracks and ground of 3.9mm.

Thanks