This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC115L: Footprint

Part Number: CC115L
Other Parts Discussed in Thread: CC1101

Hi,
Regarding the CC115L footprint, I have a question about the datasheet's PCB layout recommendations. It mentions tenting the vias on the component side of the PCB to prevent solder migration during the reflow process and advises against 100% solder paste coverage to avoid outgassing issues. However, when I checked the CAD/CAE Symbol section of the part page, the footprint includes nine vias instead of the five mentioned in the datasheet, and the vias are not tented. Which one is correct? Should the vias be tented, and should there be nine vias instead of five?



Thank you