Tool/software:
The above linked post is over a year old with no replies. I'm refreshing the questions in hopes of a response.
1. Regarding format A (2 byte sync, no preamble gating), are there register settings that will allow full range RSSI reporting without compromising RX sensitivity/BER?
2. Regarding format B (4 byte sync, with preamble gating), are there register settings that will allow full range preamble/bit detection without compromising RX sensitivity/BER or RSSI reporting?
3. What could be the reason for the slower than calculated preamble detection?