Part Number: LP-CC1352P7
Other Parts Discussed in Thread: CC1352P7, UNIFLASH, SYSCONFIG
Tool/software:
Hi all, we are dealing with an application porting from CC1352P1 to CC1352P7: with CC1352P1 OAD is running perfectly. When we try the same with CC1352P7 some issue arises:
- once a reset is issued to give control to the BIM, the application is no longer valid and control should be passed to the "persistent" application through a phsysical reset of the processor. Persistent application is exactly what we downloaded from the resource explorer, changing only the I/O used to drive the antenna switch and relative CB, exactly the same we did on the CC1352P1. It is very easy to detect the persistent is running by what is printed on the serial comm: "TI Sensor (Persistent App)" . Then the following message is printed on the OAD status line "Transferring Block 0 of 1041" and the process stalls there. That is, the persistent is completely not responding and no action can be done through the comm itself. Note this status message indicates:
- the persistent has been invoked after the reset
- the OAD process in persistent app has been correctly started
Beyond this message, all is crashed.
On the CC1352P1 with the same procedure, all is correctly running: is there any further difference? Or a different setup to get OAD functioning independently of the underlaying processor?
Thanks
Luigi