Other Parts Discussed in Thread: UNIFLASH,
Tool/software:
Hi,
I was able to run the generated standalone package on the same computer that the package was generated on, but I could not get the package to work on a different computer. After connecting the same launchpad and running the one_time_setup.bat script, I get the following error:
Connecting: fatal: Error connecting to the target, (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration is probably incorrect. (Emulation package 12.7.0.00059) failed: Operation was aborted
I tried to install UniFlash on the new computer and then download connection ccxml file:

Then replace the content in .\ccs_base\common\targetdb\connections\TIXDS110_Connection.xml with downloaded ccxml file.
Then run dsLite.bat again, I got the following output:
Executing default command: >..... DSlite version 12.7.0.3313 Configuring Debugger(may take a few minutes on first launch)... Parsing connection/TIXDS110_Connection.xml
Then nothing happens.
I guess the question is: how to determine the connection on a new computer. The quick start tool mentioned switching to a different USB connection, judging from the text, that seems to only apply to MSP430 but not CC13XX MCUs.
In case it is relevant: both computer runs Windows 11/10, the standalone package was generated by UniFlash v8.6.0.4688, a newer version of UniFlash v8.8.0.4946 was installed on the new computer to get the connection ccxml file.
So please advise.
Thanks,
ZL