This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear, We would need Declaration of conformity for these 3 parts:
CC1101RGPR
CC1150RGVR
CC1125RHBR
We would also need the EN 300 220 protocol which we need for Egyptian government organization NTRA. Will it be possible to arrange this please?
Thank you
Best regards
Pavel Motan
ELKO EP
Hi,
These devices are not modules so do not have their own Declarations of Conformity; customers follow TI's reference designs and are required to certify their products themselves. This is because customer's products will ultimately use different software and hardware (antenna, casing, ect.). Customers can use SmartRF Studio 7 to evaluate the performance of both TI hardware and custom hardware for certification using an external test house.
If the reference designs are closely followed then the designs are expected to pass regulatory requirements. The EVMs for these devices passed CE certification in order to be allowed to be sold in Europe when they were available for sale, so demonstrate that they can indeed meet the regulatory requirements.
The CC1101 EVMs are longer for sale so these DoCs are no longer available on TI.com. The CC1125DK DoC can be found here: https://www.ti.com/lit/sszqa08
Customers still need to certify their designs themselves.
Regards,
Zack