Tool/software:
Hi All,
Please tell me the recommended TCXO model number for CC1314R10.
I checked with EPSON's TG2016SMN 48.0000M-MCGNNM, but the output power is insufficient.
Best Regards,
Ito
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi All,
Please tell me the recommended TCXO model number for CC1314R10.
I checked with EPSON's TG2016SMN 48.0000M-MCGNNM, but the output power is insufficient.
Best Regards,
Ito
Hi,
Is this the case that you are reporting lower RF output power (8 dBm) when using a TCXO than when using a crystal ?
What output power do you measure with a crystal ?
Using a TCXO or a crystal should not effect the level of the RF output power.
Regards,
Richard
Hi Richard,
Since it is exactly the same hardware as EVM, the only difference is the change from crystal to TCXO.
Theo and Zack replied that there is no problem with the software.
However, we have not heard back from them since then, so please contact them.
Are there any recommended TCXO model number?
Please let us know the recommended TCXO model number.
Best Regards,
Ito
Hi,
There should not be a difference in output power when using a crystal or a TCXO. This just sets the reference frequency for the radio and not the RF output power level.
What is the voltage level to your TCXO (1.8V or 3V) ?
Are you following the SWRA640 app note Section 7 when using a TCXO: www.tij.co.jp/.../swra640
Attached TCXO datasheets that can be recommended.