Hello,
Our customer will produce sub-GHz module.
They use a combination of cc1101 and cc1190 now.
They would like to correspond to FCC15.247 without frequency hopping.
So they are trying to reference the DN006.
- DN006
http://www.ti.com/lit/an/swra123b/swra123b.pdf#search='DN006'
But CC1101 is old device.
So we would like to propose the CC1200.
Please answer following question.
1. Does the CC1200 can adapt to DN006 (design note)?
2. Is there how to increase the transmission output without the use of CC1190?
Best regards,
Manabu Ito