This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am laying out the CC1101 reference design on a 1.6 mm multilayer PCB. My previous experience is on 0.8 mm double-sided PCB. In the region of the CC1101, I have designated both internal layers as ground planes, with good stitching between the two. There is only 0.1 mm between the RF routing layer and the upper ground plane, leading to excessive capacitance on the SMD pads. If I clear this plane and use the other internal layer as ground, the distance is 1.2 mm, which is greater than the 0.8 mm of the reference design. Intuition tells me that the circuit will be happier with the upper layer as ground but how do I mitigate the pad capacitance? Is it OK to put holes in the upper ground plane under the pads to reduce the capacitance?