Dear sirs,
Our customer has a lot of devices based on CC1101/CC1100 with MSK modulation settings below:
Modulation -> MSK
Base Frequency -> 433.108917 MHz
Data Rate -> 249.939kBaud
Phase Transition Time -> 0
RX Filter BW -> 541.666667 kHz
In his new project he wants to use CC1200. It is impossible to change CC1101/CC1100 existing settings.
I tried to establish connection between CC1200 and CC1101/CC1100.
I work with TI evaluation kits :
Smart RF04EB + cc1101EM and CC120x EM + CC Debugger and SmartRF Studio 7 v2.4.2.
CC1200 settings are:
Freg -> 433.108826
RX Filter BW -> 555.555556
Modulation -> 2-FSK
Deviation -> 62.561035kHz
Symbol rate -> 249.939
I inverted the SYNC like it is mentioned on this topic:
e2e.ti.com/.../532086
I could TX Data from CC1101 and RX it in CC1200,
but I couldn't RX data in CC1101 when CC1200 TX data.
Could you please help?
How can I RX data from CC1200 in MSK mode?
Thank you for your help!