This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Our customer wants to use CC1125DK. From the 'CC1125DK Quick Start Guide', it contains only 'CC1125EM-CAT1-868' which is 868MHz.
So my question is:
Does CC1125DK contain 434MHz Module?
Thanks.
Kevin Xiong
Please take a look at Table 4.5 in the CC1125 data sheet http://www.ti.com/lit/SWRS120
to see which frequency bands are supported. 410 - 480 MHz is one of them.
You will also find links to reference designs for this band here:
Siri