Part Number: CC1101DK868-915
Hi,
we have a CC1101 device that we wish to communicate with an older existing CC1000 based product but having difficulties trying to get them to talk.
CC1101 vs CC1101 and CC1000 vs CC1000 works fine.
Have also tried receiving data on a CC1111 using packet sniffer with same key parameter settings but only able to receive data coming from CC1101.
The key parameters for the link are :
====
868.706 mhz base frequency
Channel 0
Datarate 38.4 kBaud
Channel spacing 200 khz
Deviation 32 khz
RX Filter BW set to 200 khz
2 bytes sync word 0xcb50
4 bytes preamble
16/16 bits syncwords detected
FSK-2 modulation
No FEC
No whitening
Manchester encoding
===
Remote CC1000 device uses the following register settings at startup.
MAIN 00: 11
FREQ_2A: bf
FREQ_1A: 60
FREQ_0A: 00
FREQ_2B: 58
FREQ_1B: 3d
FREQ_0B: b9
FSEP1: 01
FSEP0: ab
CURRENT: 8c
FRONT_END: 32
PA_POW: 80
PLL: 68
LOCK: 13
CAL: 26
MODEM2: c1
MODEM1: 69
MODEM0: 54
MATCH: 10
FSCTRL: 01
PRESCALER: 00
TEST4: 3f
Can someone please comment on whether there are any issues with these settings ? If additional info is required please let us know.
In an older thread on this forum (Title : "communication error between CC1000 and CC1101") there was a discussion on deviation vs freq separation on CC1000 but we have tried setting up deviation to half the freq separation of CC1000 without any success.
For reference, I am attaching the SmartRF studio register settings for CC1101 as well as the sniffer prs file used with the CC1111 when trying to sniff the packets being sent from CC1111.
Best regards,
Mattias