This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1350: CCS/CC1350 uploading firmware to an out of factory CC1350 chip

Part Number: CC1350


Tool/software: Code Composer Studio

Hi Everyone,

Has anyone tried to use 2-pin jtag interface to upload a firmware to a CC1350 at factory settings? We have tried to instead of ds110 full 5 pin interface, we rerouted VDD, gnd, nreset, TMS and TCK to the chip on our board without TDO and TDI. Is there anything that we needed to do on CC Studio or should the debugger automatically burn the BLE simple peripherals? Or do you know if it would require us to do anything for external out of factory CC1350 chip. At the moment we can't see BLE radio as opposed to the case of the chip on the Launchpad. When we burned the same way to the chip on the pad we could see BLE advertising.

Help on this is very much appreciated.

Best

Ahmet