Following up on my previous question now that I have my first boards back.
Initial BLE testing shows that connectivity is very spotty/intermittent and drops frequently. Connections can only be made when the tablet or phone is very close to the antenna. Typically 1" or less. When the tablet or phone is moved farther away, the connections drops and will not reconnect until the tablet or phone is brought back to being less than 1" away from the antenna.
As part of the troubleshooting, I discovered an error in the antenna layout. I removed the ground tie on the short leg of the antenna (as shown in the layout screen shot below). When I add a white wire tie to a nearby ground test point, performance does not change.
Two other observations in my design when I go back and compare it to the AN043 reference design I pulled the antenna from:
My board is a 6 layer 0.031" board. The AN043 board is a 4 layer 1mm (0.039") thickness.
My board house says the stackup has a dielectric constant of 4.34 at 2GHz while the AN043 calls out a dielectric constant of 4.5
As I am playing catchup in my RF theory, I am not sure how significantly those two difference will impact the performance of the BLE antenna.
I am working to get access to a network analyzer/antenna analyzer to see if I can see what the S11 reflections look like along with any other relevant tests the folks with the equipment suggest we run.
Any thoughts or suggestions are greatly appreciated!