This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI-RTOS
Hey there
I'm using CC1312R board with Linux collector application, everything works fine for me. In my application I also need OAD update that's why I followed steps to perform the OAD form the default binary files available with SDK and that's work for me
Now I need to generate the .bin of my own source .hex, that's why i just followed the steps provided here
I'm using python 2.7 along with the Intelhex, crcmod,and ecdsa
then i run the command to generate the .bin but unfortunately I haven't found .bin in my directory
python C:\Users\Mahendra\Desktop\OAD\oad/oad_image_tool.py -v 0x0200 -i Tilt_Sensor.hex -ob sensor_oad_cc13x0lp_app-nverase_v2.bin -m 0x1000
here is my cmd screenshot
Can anyone help me here ?
Thanks in Advance
Hello Gurus
I'm exacting the answers from the TI
Thanks
Thanks for your feedback
yes I'm able to generate the .bin file but for the default code only after changing the SOFTWARE_VER
but when i re-name the project from the ccs the the things not happens and i'm getting hex only!
Any advice to generate .bin after renaming of the original oad project ?
Thanks