This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My requirement is to implement Wireless Mbus to read data from water meter(T1 mode, OMSv3) using serial interface,for this purpose I am using CC1350 Launchpad EU.
Since I am first time working on TI as well as 'sub-1GHz' family I referred link "www.ti.com/.../TIDA-01531
and studied document "Low-Power wM-Bus Communications Module Reference Design" as well as application note
"Using the MSP430FR6047 Wireless M-Bus Serial Library for Metering Applications" and following are the observations:
-While studying "Low-Power wM-Bus Communications Module Reference Design", I found that 'Wireless M-Bus Suite by STACKFORCE GmbH' has been
discontinued hence was not able to implement basic communication between two CC1350 Launchpads.
-While studying "Using the MSP430FR6047 Wireless M-Bus Serial Library for Metering Applications", I found that stack is using
"Serial MAC Protocol V1"(OMSv3.0.1-compliant) for communication but documentation for WMbus-OMSv3.0.1-compliant is not available
since present "Wireless M-Bus Protocol Software" provided by TI is OMSv4.1.2 complaint with documentation available.
- Also both "Low-Power wM-Bus Communications Module Reference Design" and "Using the MSP430FR6047 Wireless M-Bus Serial Library for Metering Applications"
are not updated as per OMSv4.1.2 complaint hence I am finding difficult to communicate two CC1350 Launchpads to verify the communication.
Please provide "WMbus-OMSv3.0.1-compliant" documentation or guide me to implement basic communication between two CC1350 Launchpads using OMSv4.1.2 complaint
wMbus stack.
Hi
I have put in a request on having the App note updated.
Also, please see the attached documentation for OMSv3.0.1.
Serial_APL_interface-v3.3.5.zip
BR
Siri