This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1350: not detect device on windows PC and fail XDS110 driver installation

Part Number: LAUNCHXL-CC1350
Other Parts Discussed in Thread: CC1350, UNIFLASH,

Hi I'm WooSeok Han

I want to sniffing by CC1350 launchpad and sniffer2

not detect device on windows PC and fail XDS110 driver installation

PC OS : Windows 7 Professional K 64 bit

Installed file : ccsv 7.3.0, simplelink_cc13x0_sdk_3_10_00_11, ti_emupack_setup_8.0.903.4_win_32,

                      uniflash_sl.4.6.0.2176, WireShark 2.6.7, SmartRF_Packet_Sniffer2_1.7.0 etc

I tried installation that path

C:\ti\ccsv7\ccs_base\emulation\windows

However, the installation error message and "the specified file can not be found" are displayed.
and also, XDS110 is update complete
Please help me install the driver and detect the device.