Other Parts Discussed in Thread: CC1310, , CC1190
Hi,
We designed a custom PCB with the CC1310 following this reference design https://www.ti.com/tool/LAUNCHXL-CC13-90 and it worked great.
But because of the hardware constraints of the CC1310 we are moving our design with the CC1312R and I read that it is pin-compatible with the CC1310 but just replace the main 24mhz crystal with the 48mhz one (because of the M4F arm Cortez I assume).
Can I just change the CC1310 with the CC1312R and just change the crystal and should work just fine? What else do you recommend me to change?? because I head that the PA tables of the CC1312R are different :S.
Can I use the same power settings of the smart rf used on the CC1310 without worrying on damaging the CC1190?
Do you guys have a CC1312R-CC1190 tested design?
Thank you and good day.