Hi expert,
these days,I found similar problems in other projects.The project I am referring to is like this: using adaptive filtering for noise reduction, the filtering coefficients need to be trained in the process. I found that if the filtering coefficient training is not good, it will produce noise, which is very similar to the noise of cc1352 project.I wonder if the phenomenon of these two projects is caused by the same problem.I mean, is there some kind of filtering effect that causes this problem?