Hi team
Good day
my customer need some help:
I want to use the CC1312R as the core of a land mobile radio design - need to be able to send audio samples to the RF core for FM modulation, and received FM demodulated audio samples back - audio preferably in a g.711a/u companding (8-bit/8kHz). This will require a new "protocol" patch for the RF module as it is closed source. Separate power amplification stage, using one of the radio control GPIO pins to enable the power amplifier, and 5x other pins as a parallel bus to set the TX power level. The program core should have enough compute power to handle CTCSS and CDCSS generation and mixing with the audio data, the RF core has more than enough compute power to modulate analog audio if it is computing gaussian functions on 4-level digital states. Extra functions for the display and user control IO are low enough rate for a state machine in a light CPLD. This should be possible, and I want to get there first. CC1312R is interesting as it covers the two bands I'm targeting (MURS/GMRS).
Best regards
Aosker