This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3XXXRADIOTEST: CC31xx/32xx RadiotoolGUI v1.0.3.18

Part Number: CC3XXXRADIOTEST
Other Parts Discussed in Thread: UNIFLASH, CC31XXEMUBOOST, CC3130,

Hi Experts,

My customer is having problems installing the Radio tool on a win7 computer. He have installed Uniflash version 7.2.0.3893 for flashing, this part works.

The board he is using works perfectly on 2 other PCs, both of these installed with win10.

To control Radio measurements he want to use RadiotoolGUI v1.0.3.18 in the UART mode connecting via CC31XXEMUBOOST

Selects UART CC3130
Select item 13 (comport range 11..14)
clicking the connect i immediately gets connection error, looks like no access to com ports, (tried blocking port on working PC) the win7 PC has no other programs running so port should be available.

They are about to send a device for FCC and EU measurements, to setup the CC3130 we will use the CC3xxxRadiotest along with an PC.

Error message please see below screen shot


I hope you can help us. Thank you.

Kind regards,
Gerald