This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3135: Application issues of chips

Part Number: CC3135

I encountered the following problem while debugging CC3135. Can you help me answer it.

We use SOP0 and SOP1 as control pins for switching between 5Gwifi TX and RX switches.

However, when testing 5GWIFI, we found that while the MCU was communicating with CC3135, the output levels of SOP0 and SOP1 were 92mv

However, when the communication between MCU and CC3135 is disconnected, and the PC is connected to the EMU board, and the EMU board is connected to

CC3135 (with TX, RX, GND, NHIB, RTS, CTS ports), the output levels of SOP0 and SOP1 are 3.3v.

May I ask what is the reason for this phenomenon? Is there any configuration that hasn't been done? How can I solve these problems?