Tool/software:
Hi,
This is follow up question from the previous post.
In the original thread, below answer was provided.
> Its not possible to completely turn off 2.4GHz but you can scan for only 2.4Ghz or 5GHz and those connections will use the their corresponding mode.
> You can however disable 5GHz
Even if 2.4GHz is masked in scan policy, this does not mean 2.4GHz radio is not transmitted during scan.
Scan results of 2.4GHz are masked and not used for connection. Correct?
Thanks and regards,
Koichiro Tashiro