This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3301: Connect to a special AP(wpa/wpa2) failed.(R5 version)

Part Number: CC3301

Tool/software:

cc3301 always unable to connect to a specific AP, the information of this AP is as follows:

AP type: TP Link Deco M9(https://www.tp-link.com/se/home-networking/deco/deco-m9-plus/v1%20(1-pack)/)

Through packet capturing, we can see that after the four-way handshake, the cc3301 initiates the disconnection for unknown reasons.

  • Hello Similar to the precious thread, can you please provide some FW logs?

    We are working on some potential fix but we would like to make sure we have all of the information.

  • Hi AB

    The CC33 trace: carrot-ispteam-r5-connect-fail-cc33.pcap


    And a 802.11 trace: carrot-ispteam-fail-r5.pcap-01.cap

    carrot-ispteam-fail-r5.pcap-01.cap.logcarrot-ispteam-r5-connect-fail-cc33.pcap.log

  • Hi,

    The cc33xx trace is no good since the logger.bin parser is not the right one. See my other thread where I directed you to the right logger.bin.

    The air sniffer is just full of RTS, CTS and ACK. I don't see any beacons from AP or station trying to scan and connect. Please make sure you see the beacons from the AP first.

    Shlomi

  • 我也遇到了同样的问题,在连接WPA3时也有问题,最后也没解决!

  • Please check this file, there is a beacon package in it.

    8551.cc3301_1.pcap.log
    �ò���i:n#gԳCC�������~ڈ���~ڈ���p����w�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3���������L��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���An#g˚!!P:`���~ڈ���~ڈ�����sKWx�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���An#g��
    
    �~ڈ���An#g�!!P:`���~ڈ���~ڈ������VWx�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���An#g�
    
    �~ڈ���Bn#g��	!!P:`���~ڈ���~ڈ�������gx�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���Bn#g��	
    
    �~ڈ���Bn#g<�	!!P:`���~ڈ���~ڈ�����V�gx�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���Bn#g��	!!P:`���~ڈ���~ڈ������gx�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���Bn#g
    
    !!P:`���~ڈ���~ڈ������gx�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���Bn#g�
    
    
    �E`���Bn#g�
    rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ Bn#g�
    
    
    �`���Bn#gI�
    !!P:`���~ڈ���~ڈ������whx�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���Bn#gۅ
    
    
    �~ڈ���Bn#g`2�~ڈ���`���~ڈ���Bn#g33�~ڈ���`���~ڈ���Bn#gO3
    
    �`���Bn#g�A�:`���~ڈ���~ڈ�����Bn#g�B
    
    �~ڈ���Bn#g�D��,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�Bn#g�D
    
    �`���Bn#g��\\B������~ڈ���tڈ���0ll�`��fZC�-w���p`�� 9�7/���V+c����y՘�Zb���1�����oXL�Bn#g�2��:`���~ڈ���~ڈ�����1�����$20H`lFs�-�	��=@�P���'�BC^b2/����~ڈ���Bn#g
    4
    
    �~ڈ���Bn#g�t���:`���~ڈ���~ڈ�������_��?εpm+��1����׸��e#ɴa�ܶBn#g�u
    
    �~ڈ���Bn#g�y���,~ڈ���`���~ڈ�������u
    ���������������������������������F䬂�>E���1��0���Bn#g�y
    
    �`���Bn#g_����:`���~ڈ���~ڈ����������?εpm+��1����׸��e#ɴa�ܶcm`�
    �n���C���hf�<���9��‹]w�9++������>���q�`�M��rc슕������8Kl�����OE�������yt��u��1Qt��A��i�X�o&ҏy<_�h�Bn#gk�
    
    �~ڈ���Bn#g�����,~ڈ���`���~ڈ�������_
    ������I��_�Bn#g��
    
    �`���Bn#gٿ���	,~ڈ���`���~ڈ�������_
    ������I��_�Bn#g�
    
    �`���Bn#g���~ڈ���`���~ڈ���0Bn#g��~ڈ���`���~ڈ���0Bn#g���~ڈ���`���~ڈ���0Bn#gl��<~ڈ���`���~ڈ���0Bn#g��
    
    �`���fn#g�.
    !!P:lG`�'~ڈ���~ڈ�����Mq�z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���fn#g�/
    
    
    �~ڈ���in#g2�!!P:`���~ڈ���~ڈ����W߼z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���in#g��!!P:`���~ڈ���~ڈ�����z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���in#g��!!P:`���~ڈ���~ڈ�����z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���in#g��!!P:`���~ڈ���~ڈ�����z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���in#g��
    
    �~ڈ���in#gU�!!P:`���~ڈ���~ڈ��� �u��z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���in#gV�
    
    �~ڈ���jn#g"�
    !!P:`���~ڈ���~ڈ���0�_�z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���jn#g �
    
    
    �~ڈ���jn#g��
    !!P:`���~ڈ���~ڈ���@���z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���jn#g��
    
    
    �~ڈ���jn#g��
    
    
    �,`���jn#g$Lrr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ jn#g?L
    
    �`���jn#g�W!!P:`���~ڈ���~ڈ���P帢�z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���jn#gmX
    
    �~ڈ���jn#g��~ڈ���`���~ڈ���jn#g�
    
    �`���jn#g��:`���~ڈ���~ڈ���`�jn#g�
    
    �~ڈ���jn#g���,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�jn#g
    
    �`���kn#g����:`���~ڈ���~ڈ���p�1�����$20H`lFs�-�	��=@�P���'�BC^b2/����~ڈ���kn#ga�
    
    �~ڈ���kn#gI����:`���~ڈ���~ڈ�������_�)z�Wu5.�vY��
    �›\.b�!>{�y׮���kn#g=�
    
    �~ڈ���kn#gS����,~ڈ���`���~ڈ�������u
    	
    
     !"$%&'3b�L��<4�J�P?V0���kn#gj�
    
    �`���kn#g((���:`���~ڈ���~ڈ���������)z�Wu5.�vY��
    �›\.b�!>{�y׮����T�LcO���"vNh���U�3+$�.�������C��*���"��V��aY���Zlj�?�L�:�����j��5�������k��V�3���q6!$�����+d�B礩q�Jkn#g�(
    
    �~ڈ���kn#gE.���,~ڈ���`���~ڈ�������_
    �R��j)�g�.�J���kn#g\.
    
    �`���kn#g�0�~ڈ���`���~ڈ���0kn#g1
    
    �`���kn#gs�!!P:t�C(�~ڈ���~ڈ������S�z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���kn#g"�!!P:t�C(�~ڈ���~ڈ�����h�z�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���kn#g*�
    
    �~ڈ���n#g�x!!P:��;��~ڈ���~ڈ������1|�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���n#g�y
    
    �~ڈ���n#g��!!P:��;��~ڈ���~ڈ������C|�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���n#gN�
    
    �~ڈ���n#gM�!!P:��;��~ڈ���~ڈ�����h�|�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���n#g��!!P:��;��~ڈ���~ڈ�����ˑ|�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���n#g��!!P:��;��~ڈ���~ڈ�����,�|�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���n#g��!!P:��;��~ڈ���~ڈ�������	|�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���n#g��
    
    �~ڈ���n#g2%	!!P:��;��~ڈ���~ڈ�����y�	|�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���n#g�4	!!P:��;��~ڈ���~ڈ�������	|�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���n#g?	!!P:��;��~ڈ���~ڈ�����S�	|�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g�W!!P:`���~ڈ���~ڈ�������#}�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#gY
    
    �~ڈ����n#gfc!!P:`���~ڈ���~ڈ�����U$}�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g�d
    
    �~ڈ����n#gD�!!P:`���~ڈ���~ڈ������3}�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g>�!!P:`���~ڈ���~ڈ�����3}�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g��!!P:`���~ڈ���~ڈ������4}�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g��
    
    �~ڈ����n#g��!!P:`���~ڈ���~ڈ��� ��4}�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g�!!P:`���~ڈ���~ڈ��� ���4}�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g�
    
    �du`����n#g�}rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ �n#g�}
    
    �`����n#gz�rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ �n#g��
    
    �`����n#g�!!P:`���~ڈ���~ڈ���0��5}�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g��
    
    �~ڈ����n#g��~ڈ���`���~ڈ����n#g�
    
    �`����n#g�+�:`���~ڈ���~ڈ���@��n#g-
    
    �~ڈ����n#g*/��,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P��n#g3/
    
    �`����n#g*��:`���~ڈ���~ڈ���P�1�����$20H`lFs�-�	��=@�P���'�BC^b2/����~ڈ����n#g+
    
    �~ڈ����n#g�P���:`���~ڈ���~ڈ�������_��\���tu_��yM
    h���׵1�L�����B��n#g�Q
    
    �~ڈ����n#g�U���,~ڈ���`���~ڈ�������u
    bdefghiklmnoqrstuvxyz{|}�������oۖI$&|U$�G��0����n#g�U
    
    �`����n#g~����:`���~ڈ���~ڈ����������\���tu_��yM
    h���׵1�L�����B�Ҽ���e��Z�c�;h��r�rݣ�N��?�hn��`r��h�0���l�Ū`�R�տlۜ\��"�u�^�`S!l�O��#�g�Gq�{�T�D�]e>�O������C�-��L���CD����n#g��
    
    �~ڈ����n#gޜ���,~ڈ���`���~ڈ�������_
    �(�>6��7�M��w�n#g�
    
    �`����n#gR��~ڈ���`���~ڈ���0�n#g[�
    
    �`����n#g��!!P:t�C(�~ڈ���~ڈ���`�'t~�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g�!!P:t�C(�~ڈ���~ڈ���`�1t~�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g:�!!P:t�C(�~ڈ���~ڈ���`�Gt~�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g��
    
    �~ڈ����n#g�!!P:lG`�'~ڈ���~ڈ���p�~�E�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g,�
    
    �~ڈ����n#g�4
    !!P:�]d�p~ڈ���~ڈ�����h��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g6
    
    
    �~ڈ����n#g��!!P::}�[~ڈ���~ڈ������[��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g:�!!P::}�[~ڈ���~ڈ�����{�[��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g��!!P::}�[~ڈ���~ڈ������[��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g��!!P::}�[~ڈ���~ڈ�����ȴ_��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g��!!P::}�[~ڈ���~ڈ�����,�_��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g��
    
    �~ڈ����n#gdM!!P::}�[~ڈ���~ڈ�����O`��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g2b!!P::}�[~ڈ���~ڈ�����\d`��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g,c
    
    �~ڈ����n#g;�!!P::}�[~ڈ���~ڈ�����*]���d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g�Y!!P::}�[~ڈ���~ڈ���������d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#ggn!!P::}�[~ڈ���~ڈ�����j���d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g�!!P:��;��~ڈ���~ڈ������b/��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g/�
    
    �~ڈ����n#g��!!P:��;��~ڈ���~ڈ�����Dn/��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g��
    
    �~ڈ����n#gF�!!P:��;��~ڈ���~ڈ������/��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g�!!P:��;��~ڈ���~ڈ����ز0��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g5	!!P:��;��~ڈ���~ڈ������0��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ����n#g�
    	!!P:��;��~ڈ���~ڈ����J�0��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#g��!!P:lG`�'~ڈ���~ڈ����+����d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#g��
    
    �~ڈ���o#g7j!!P:`���~ڈ���~ڈ��� �-nք�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#g?k
    
    �~ڈ���o#g�~!!P:`���~ڈ���~ڈ���0��ք�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#g �
    
    �~ڈ���o#gK�!!P:`���~ڈ���~ڈ���@����d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#gd�
    
    �~ڈ���o#gb�!!P:`���~ڈ���~ڈ���P����d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#gϡ!!P:`���~ڈ���~ڈ���P����d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#g.�!!P:`���~ڈ���~ڈ���P�s���d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#g�
    
    �E`���o#g�rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ o#g�
    
    �`���o#g�%!!P:`���~ڈ���~ڈ���`�'l��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#g'
    
    �~ڈ���o#gI��~ڈ���`���~ڈ���o#gR�
    
    �`���o#g���~ڈ���`���~ڈ���o#g��
    
    �`���o#g:��:`���~ڈ���~ڈ���p�o#gb�
    
    �~ڈ���o#g����,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�o#g��
    
    �`���o#g����:`���~ڈ���~ڈ�����1�����$20H`lFs�-�	��=@�P���'�BC^b2/����~ڈ���o#g��
    
    �~ڈ���o#g����:`���~ڈ���~ڈ�������_����W\Z2�ܑ���̾��h��;I�b���
    �o#g2�
    
    �~ڈ���o#g����,~ڈ���`���~ڈ�������u
    
    
     !"#%&'P��²5J%��?ハ0���o#g#�
    
    �`���o#g�1���:`���~ڈ���~ڈ������������W\Z2�ܑ���̾��h��;I�b���
    ��G4Z}r㕜h�'�� �hמK!Y�C$��M�=���rp�q׊jW>�/�܉EY�렴���gY��tLR���o�*�ȃ� ޔ�%C/qO:��R]�/Vy�:��-��i�'�u�A�o#g�2
    
    �~ڈ���o#g:8���,~ڈ���`���~ڈ�������_
    L9��6�s��b{���o#gC8
    
    �`���o#g�:�~ڈ���`���~ڈ���0o#g�:
    
    �`���o#gW�!!P:t�C(�~ڈ���~ڈ�����	���d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#g��!!P:t�C(�~ڈ���~ڈ��������d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���o#g!!P:t�C(�~ڈ���~ڈ�����y���d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���;o#g�w!!P:`���~ڈ���~ڈ�����^�<��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���;o#gH�!!P:`���~ڈ���~ڈ�������<��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���;o#g]�!!P:`���~ڈ���~ڈ�������<��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���;o#g��!!P:`���~ڈ���~ڈ������<��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���;o#g�!!P:`���~ڈ���~ڈ�����b=��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���;o#g��!!P:`���~ڈ���~ڈ�����A��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���;o#g��
    
    �~ڈ���;o#g��!!P:`���~ڈ���~ڈ�����A��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���;o#g��
    
    �~ڈ���<o#g�D
    !!P:`���~ڈ���~ڈ�����[�Q��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���<o#g�E
    
    
    �~ڈ���<o#g�S
    !!P:`���~ڈ���~ڈ�����>�Q��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���<o#g�a
    !!P:`���~ڈ���~ڈ�����R��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���<o#g�x
    
    
    �~ڈ���<o#g�x
    
    
    ��t`���<o#g��
    rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ <o#g��
    
    
    �`���<o#g�!!P:`���~ڈ���~ڈ���譡R��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���<o#g3
    
    �~ڈ���<o#g\��~ڈ���`���~ڈ���<o#gf�
    
    �`���<o#g���:`���~ڈ���~ڈ����<o#g��
    
    �~ڈ���<o#g����,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�<o#g��
    
    �`���=o#g�C��:`���~ڈ���~ڈ��� �1�����$20H`lFs�-�	��=@�P���'�BC^b2/����~ڈ���=o#g�D
    
    �~ڈ���=o#g9y���:`���~ڈ���~ڈ�������_�LgՎ�ȉ9@S�|jc����@'�H�+o1���=o#gZz
    
    �~ڈ���=o#g<~���,~ڈ���`���~ڈ�������u
     !"$%&'()+,-./12345689:;<=_g�N�٠�d&�!)Q�0���=o#gE~
    
    �`���=o#g�����:`���~ڈ���~ڈ���������LgՎ�ȉ9@S�|jc����@'�H�+o1���Z�S���06m���h�����^E}�&�j	��j"�_�Q�ԗ���VU.X����-<��Ɩ���J��F*�pXO�H�Z�^��#�$%�먴��fR O�g�����ͪ���-=o#g��
    
    �~ڈ���=o#g;����,~ڈ���`���~ڈ�������_
    H0�ûJ�2p�%k=o#g|�
    
    �`���=o#g���~ڈ���`���~ڈ���0=o#g��
    
    �`���To#g
    V!!P:lG`�'~ڈ���~ڈ���0�)���d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���To#g/W
    
    �~ڈ���do#g|�!!P:`���~ڈ���~ڈ���@�􉧉�d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���do#gm�
    
    �~ڈ���do#gȞ!!P:`���~ڈ���~ڈ���P�d����d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���do#g�
    
    �~ڈ���eo#gg�!!P:`���~ڈ���~ڈ���`�D����d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���eo#gq�
    
    �~ڈ���eo#g��!!P:`���~ڈ���~ڈ���p�y���d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���eo#g��!!P:`���~ڈ���~ڈ���p��#���d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���eo#g��
    
    �z`���eo#gVVrr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ eo#g_V
    
    �`���eo#g�{!!P:`���~ڈ���~ڈ�����q����d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���eo#g�|
    
    �~ڈ���eo#g���~ڈ���`���~ڈ���eo#g��
    
    �`���eo#gD�:`���~ڈ���~ڈ�����eo#gm
    
    �~ڈ���eo#g
    ��,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�eo#g
    
    
    �`���eo#gO
    
    �~ڈ���eo#g(���:`���~ڈ���~ڈ�������_�a�δ�iO-\U�.C��$��e���P����eo#g+)
    
    �~ڈ���eo#g�-���,~ڈ���`���~ڈ�������u
    ����������������������	
    J�W�;2����0���eo#g�-
    
    �`���eo#g�-���	,~ڈ���`���~ڈ�������u
    ����������������������	
    J�W�;2����0���eo#g�-
    
    �`���eo#g�n���:`���~ڈ���~ڈ���������a�δ�iO-\U�.C��$��e���P����S��^��FT��Y��h�TP�svȡ�׷eJÃ�V��K�C���l�n�#��[+HRZ�\�vh0QM��˩�j�������/h?vK���G
    	ԗy�cmE�S����������xeo#g�o
    
    �~ڈ���eo#gW|���,~ڈ���`���~ڈ�������_
    D���^'R��+�eo#g`|
    
    �`���eo#g�}�~ڈ���`���~ڈ���0eo#g�}
    
    �`���oo#g�w!!P:��;��~ڈ���~ڈ�����7FU��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g*�!!P:��;��~ڈ���~ڈ������XU��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g��!!P:��;��~ڈ���~ڈ�����,oU��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#ge�!!P:��;��~ڈ���~ڈ�����}U��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g��!!P:��;��~ڈ���~ڈ�����q�U��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g/�!!P:��;��~ڈ���~ڈ�����ՑU��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#gS�!!P:��;��~ڈ���~ڈ������}V��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g\�
    
    �~ڈ���oo#g��!!P:��;��~ڈ���~ڈ�����w�V��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g�!!P:��;��~ڈ���~ڈ������V��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g:!!P:��;��~ڈ���~ڈ�������V��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g�6!!P:��;��~ڈ���~ڈ������W��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#gnA!!P:��;��~ڈ���~ڈ�����W��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g�M!!P:��;��~ڈ���~ڈ�����PW��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#gB�!!P:��;��~ڈ���~ڈ�������W��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���oo#g�$	!!P:��;��~ڈ���~ڈ������W��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���|o#gd-!!P:~Kԝ�[~ڈ���~ڈ����iX��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���|o#g�C!!P:~Kԝ�[~ڈ���~ڈ����n��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���|o#g?O!!P:~Kԝ�[~ڈ���~ڈ����`z��d1ispteam����$DE 
    *20H`lFs�-���=@��Y�3��������P���'�BC^b2/�	��P�P�P�P�P�0��������~ڈ���

  • We don't have wpa3 connection issue.

  • it is just a single beacon.

    where is all the beacons, authentication, association, EAPOL, etc...

    either you are not on the right channel or it is filtered.

  • there is EAPOL, association, authentication and deauthentication, can you see it?

  • Hi,

    Sorry, I must have missed it.

    The reason it is not able to connect is because the AP is configured to mixed mode security, i.e. TKIP+AES. See screenshot:

    In the release note, we declare support of OPEN, WPA2 and WPA3 (not WPA mixed mode).

    In the MPU side with the same chip, we did add this support so at some point I believe that it would be also added to the ThickMAC but I do not have a schedule.

    Shlomi