This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
cc3301 always unable to connect to a specific AP, the information of this AP is as follows:
AP type: TP Link Deco M9(https://www.tp-link.com/se/home-networking/deco/deco-m9-plus/v1%20(1-pack)/)
Through packet capturing, we can see that after the four-way handshake, the cc3301 initiates the disconnection for unknown reasons.
Hi AB
The CC33 trace: carrot-ispteam-r5-connect-fail-cc33.pcap
And a 802.11 trace: carrot-ispteam-fail-r5.pcap-01.cap
carrot-ispteam-fail-r5.pcap-01.cap.logcarrot-ispteam-r5-connect-fail-cc33.pcap.log
Hi,
The cc33xx trace is no good since the logger.bin parser is not the right one. See my other thread where I directed you to the right logger.bin.
The air sniffer is just full of RTS, CTS and ACK. I don't see any beacons from AP or station trying to scan and connect. Please make sure you see the beacons from the AP first.
Shlomi
Please check this file, there is a beacon package in it.
�ò���i:n#gԳCC�������~ڈ���~ڈ���p����w�d1ispteam����$DE *20H`lFs�-���=@��Y�3���������L��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���An#g˚!!P:`���~ڈ���~ڈ�����sKWx�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���An#g�� �~ڈ���An#g�!!P:`���~ڈ���~ڈ������VWx�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���An#g� �~ڈ���Bn#g�� !!P:`���~ڈ���~ڈ�������gx�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���Bn#g�� �~ڈ���Bn#g<� !!P:`���~ڈ���~ڈ�����V�gx�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���Bn#g�� !!P:`���~ڈ���~ڈ������gx�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���Bn#g !!P:`���~ڈ���~ڈ������gx�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���Bn#g� �E`���Bn#g� rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ Bn#g� �`���Bn#gI� !!P:`���~ڈ���~ڈ������whx�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���Bn#gۅ �~ڈ���Bn#g`2�~ڈ���`���~ڈ���Bn#g33�~ڈ���`���~ڈ���Bn#gO3 �`���Bn#g�A�:`���~ڈ���~ڈ�����Bn#g�B �~ڈ���Bn#g�D��,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�Bn#g�D �`���Bn#g��\\B������~ڈ���tڈ���0ll�`��fZC�-w���p`�� 9�7/���V+c����y�Zb���1�����oXL�Bn#g�2��:`���~ڈ���~ڈ�����1�����$20H`lFs�-� ��=@�P���'�BC^b2/����~ڈ���Bn#g 4 �~ڈ���Bn#g�t���:`���~ڈ���~ڈ�������_��?εpm+��1������e#ɴa�ܶBn#g�u �~ڈ���Bn#g�y���,~ڈ���`���~ڈ�������u ���������������������������������F䬂�>E���1��0���Bn#g�y �`���Bn#g_����:`���~ڈ���~ڈ����������?εpm+��1������e#ɴa�ܶcm`� �n���C���hf�<���9��]w�9++������>���q�`�M��rc슕������8Kl�����OE�������yt��u��1Qt��A��i�X�o&ҏy<_�h�Bn#gk� �~ڈ���Bn#g�����,~ڈ���`���~ڈ�������_ ���И���I��_�Bn#g�� �`���Bn#gٿ��� ,~ڈ���`���~ڈ�������_ ���И���I��_�Bn#g� �`���Bn#g���~ڈ���`���~ڈ���0Bn#g��~ڈ���`���~ڈ���0Bn#g���~ڈ���`���~ڈ���0Bn#gl��<~ڈ���`���~ڈ���0Bn#g�� �`���fn#g�. !!P:lG`�'~ڈ���~ڈ�����Mq�z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���fn#g�/ �~ڈ���in#g2�!!P:`���~ڈ���~ڈ����Wz�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���in#g��!!P:`���~ڈ���~ڈ�����z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���in#g��!!P:`���~ڈ���~ڈ�����z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���in#g��!!P:`���~ڈ���~ڈ�����z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���in#g�� �~ڈ���in#gU�!!P:`���~ڈ���~ڈ��� �u��z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���in#gV� �~ڈ���jn#g"� !!P:`���~ڈ���~ڈ���0�_�z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���jn#g � �~ڈ���jn#g�� !!P:`���~ڈ���~ڈ���@���z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���jn#g�� �~ڈ���jn#g�� �,`���jn#g$Lrr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ jn#g?L �`���jn#g�W!!P:`���~ڈ���~ڈ���P帢�z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���jn#gmX �~ڈ���jn#g��~ڈ���`���~ڈ���jn#g� �`���jn#g��:`���~ڈ���~ڈ���`�jn#g� �~ڈ���jn#g���,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�jn#g �`���kn#g����:`���~ڈ���~ڈ���p�1�����$20H`lFs�-� ��=@�P���'�BC^b2/����~ڈ���kn#ga� �~ڈ���kn#gI����:`���~ڈ���~ڈ�������_�)z�Wu5.�vY�� �\.b�!>{�y���kn#g=� �~ڈ���kn#gS����,~ڈ���`���~ڈ�������u !"$%&'3b�L��<4�J�P?V0���kn#gj� �`���kn#g((���:`���~ڈ���~ڈ���������)z�Wu5.�vY�� �\.b�!>{�y����T�LcO���"vNh���U�3+$�.�������C��*���"��V��aY���Zlj�?�L�:�����j��5�������k��V�3���q6!$�����+d�B礩q�Jkn#g�( �~ڈ���kn#gE.���,~ڈ���`���~ڈ�������_ �R��j)�g�.�J���kn#g\. �`���kn#g�0�~ڈ���`���~ڈ���0kn#g1 �`���kn#gs�!!P:t�C(�~ڈ���~ڈ������S�z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���kn#g"�!!P:t�C(�~ڈ���~ڈ�����h�z�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���kn#g*� �~ڈ���n#g�x!!P:��;��~ڈ���~ڈ������1|�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���n#g�y �~ڈ���n#g��!!P:��;��~ڈ���~ڈ������C|�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���n#gN� �~ڈ���n#gM�!!P:��;��~ڈ���~ڈ�����h�|�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���n#g��!!P:��;��~ڈ���~ڈ�����ˑ|�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���n#g��!!P:��;��~ڈ���~ڈ�����,�|�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���n#g��!!P:��;��~ڈ���~ڈ������� |�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���n#g�� �~ڈ���n#g2% !!P:��;��~ڈ���~ڈ�����y� |�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���n#g�4 !!P:��;��~ڈ���~ڈ������� |�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���n#g? !!P:��;��~ڈ���~ڈ�����S� |�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�W!!P:`���~ڈ���~ڈ�������#}�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#gY �~ڈ����n#gfc!!P:`���~ڈ���~ڈ�����U$}�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�d �~ڈ����n#gD�!!P:`���~ڈ���~ڈ������3}�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g>�!!P:`���~ڈ���~ڈ�����3}�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g��!!P:`���~ڈ���~ڈ������4}�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�� �~ڈ����n#g��!!P:`���~ڈ���~ڈ��� ��4}�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�!!P:`���~ڈ���~ڈ��� ���4}�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g� �du`����n#g�}rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ �n#g�} �`����n#gz�rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ �n#g�� �`����n#g�!!P:`���~ڈ���~ڈ���0��5}�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�� �~ڈ����n#g��~ڈ���`���~ڈ����n#g� �`����n#g�+�:`���~ڈ���~ڈ���@��n#g- �~ڈ����n#g*/��,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P��n#g3/ �`����n#g*��:`���~ڈ���~ڈ���P�1�����$20H`lFs�-� ��=@�P���'�BC^b2/����~ڈ����n#g+ �~ڈ����n#g�P���:`���~ڈ���~ڈ�������_��\���tu_��yM h���1�L�����B��n#g�Q �~ڈ����n#g�U���,~ڈ���`���~ڈ�������u bdefghiklmnoqrstuvxyz{|}�������oۖI$&|U$�G��0����n#g�U �`����n#g~����:`���~ڈ���~ڈ����������\���tu_��yM h���1�L�����B�Ҽ���e��Z�c�;h��r�rݣ�N��?�hn��`r��h�0���l�Ū`�R�տlۜ\��"�u�^�`S!l�O��#�g�Gq�{�T�D�]e>�O������C�-��L���CD����n#g�� �~ڈ����n#gޜ���,~ڈ���`���~ڈ�������_ �(�>6��7�M��w�n#g� �`����n#gR��~ڈ���`���~ڈ���0�n#g[� �`����n#g��!!P:t�C(�~ڈ���~ڈ���`�'t~�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�!!P:t�C(�~ڈ���~ڈ���`�1t~�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g:�!!P:t�C(�~ڈ���~ڈ���`�Gt~�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�� �~ڈ����n#g�!!P:lG`�'~ڈ���~ڈ���p�~�E�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g,� �~ڈ����n#g�4 !!P:�]d�p~ڈ���~ڈ�����h��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g6 �~ڈ����n#g��!!P::}�[~ڈ���~ڈ������[��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g:�!!P::}�[~ڈ���~ڈ�����{�[��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g��!!P::}�[~ڈ���~ڈ������[��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g��!!P::}�[~ڈ���~ڈ�����ȴ_��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g��!!P::}�[~ڈ���~ڈ�����,�_��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�� �~ڈ����n#gdM!!P::}�[~ڈ���~ڈ�����O`��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g2b!!P::}�[~ڈ���~ڈ�����\d`��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g,c �~ڈ����n#g;�!!P::}�[~ڈ���~ڈ�����*]���d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�Y!!P::}�[~ڈ���~ڈ���������d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#ggn!!P::}�[~ڈ���~ڈ�����j���d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�!!P:��;��~ڈ���~ڈ������b/��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g/� �~ڈ����n#g��!!P:��;��~ڈ���~ڈ�����Dn/��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�� �~ڈ����n#gF�!!P:��;��~ڈ���~ڈ������/��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g�!!P:��;��~ڈ���~ڈ����ز0��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g5 !!P:��;��~ڈ���~ڈ������0��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ����n#g� !!P:��;��~ڈ���~ڈ����J�0��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#g��!!P:lG`�'~ڈ���~ڈ����+����d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#g�� �~ڈ���o#g7j!!P:`���~ڈ���~ڈ��� �-nք�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#g?k �~ڈ���o#g�~!!P:`���~ڈ���~ڈ���0��ք�d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#g � �~ڈ���o#gK�!!P:`���~ڈ���~ڈ���@����d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#gd� �~ڈ���o#gb�!!P:`���~ڈ���~ڈ���P����d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#gϡ!!P:`���~ڈ���~ڈ���P����d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#g.�!!P:`���~ڈ���~ڈ���P�s���d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#g� �E`���o#g�rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ o#g� �`���o#g�%!!P:`���~ڈ���~ڈ���`�'l��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#g' �~ڈ���o#gI��~ڈ���`���~ڈ���o#gR� �`���o#g���~ڈ���`���~ڈ���o#g�� �`���o#g:��:`���~ڈ���~ڈ���p�o#gb� �~ڈ���o#g����,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�o#g�� �`���o#g����:`���~ڈ���~ڈ�����1�����$20H`lFs�-� ��=@�P���'�BC^b2/����~ڈ���o#g�� �~ڈ���o#g����:`���~ڈ���~ڈ�������_����W\Z2�ܑ���̾��h��;I�b��� �o#g2� �~ڈ���o#g����,~ڈ���`���~ڈ�������u !"#%&'P��²5J%��?ハ0���o#g#� �`���o#g�1���:`���~ڈ���~ڈ������������W\Z2�ܑ���̾��h��;I�b��� ��G4Z}r㕜h�'�� �hמK!Y�C$��M�=���rp�qjW>�/�܉EY�렴���gY��tLR���o�*�ȃ� ޔ�%C/qO:��R]�/Vy�:��-��i�'�u�A�o#g�2 �~ڈ���o#g:8���,~ڈ���`���~ڈ�������_ L9��6�s��b{���o#gC8 �`���o#g�:�~ڈ���`���~ڈ���0o#g�: �`���o#gW�!!P:t�C(�~ڈ���~ڈ����� ���d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#g��!!P:t�C(�~ڈ���~ڈ��������d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���o#g!!P:t�C(�~ڈ���~ڈ�����y���d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���;o#g�w!!P:`���~ڈ���~ڈ�����^�<��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���;o#gH�!!P:`���~ڈ���~ڈ�������<��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���;o#g]�!!P:`���~ڈ���~ڈ�������<��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���;o#g��!!P:`���~ڈ���~ڈ������<��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���;o#g�!!P:`���~ڈ���~ڈ�����b=��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���;o#g��!!P:`���~ڈ���~ڈ�����A��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���;o#g�� �~ڈ���;o#g��!!P:`���~ڈ���~ڈ�����A��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���;o#g�� �~ڈ���<o#g�D !!P:`���~ڈ���~ڈ�����[�Q��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���<o#g�E �~ڈ���<o#g�S !!P:`���~ڈ���~ڈ�����>�Q��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���<o#g�a !!P:`���~ڈ���~ڈ�����R��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���<o#g�x �~ڈ���<o#g�x ��t`���<o#g�� rr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ <o#g�� �`���<o#g�!!P:`���~ڈ���~ڈ���譡R��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���<o#g3 �~ڈ���<o#g\��~ڈ���`���~ڈ���<o#gf� �`���<o#g���:`���~ڈ���~ڈ����<o#g�� �~ڈ���<o#g����,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�<o#g�� �`���=o#g�C��:`���~ڈ���~ڈ��� �1�����$20H`lFs�-� ��=@�P���'�BC^b2/����~ڈ���=o#g�D �~ڈ���=o#g9y���:`���~ڈ���~ڈ�������_�LgՎ�ȉ9@S�|jc����@'�H�+o1���=o#gZz �~ڈ���=o#g<~���,~ڈ���`���~ڈ�������u !"$%&'()+,-./12345689:;<=_g�N�٠�d&�!)Q�0���=o#gE~ �`���=o#g�����:`���~ڈ���~ڈ���������LgՎ�ȉ9@S�|jc����@'�H�+o1���Z�S���06m���h�����^E}�&�j ��j"�_�Q�ԗ���VU.X����-<��Ɩ���J��F*�pXO�H�Z�^��#�$%�먴��fR O�g�����ͪ���-=o#g�� �~ڈ���=o#g;����,~ڈ���`���~ڈ�������_ H0�ûJ�2p�%k=o#g|� �`���=o#g���~ڈ���`���~ڈ���0=o#g�� �`���To#g V!!P:lG`�'~ڈ���~ڈ���0�)���d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���To#g/W �~ڈ���do#g|�!!P:`���~ڈ���~ڈ���@��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���do#gm� �~ڈ���do#gȞ!!P:`���~ڈ���~ڈ���P�d����d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���do#g� �~ڈ���eo#gg�!!P:`���~ڈ���~ڈ���`�D����d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���eo#gq� �~ڈ���eo#g��!!P:`���~ڈ���~ڈ���p�y���d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���eo#g��!!P:`���~ڈ���~ڈ���p��#���d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���eo#g�� �z`���eo#gVVrr@�~ڈ���`���~ڈ���ispteam��������2����- �H�#@�����@ eo#g_V �`���eo#g�{!!P:`���~ڈ���~ڈ�����q����d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���eo#g�| �~ڈ���eo#g���~ڈ���`���~ڈ���eo#g�� �`���eo#gD�:`���~ڈ���~ڈ�����eo#gm �~ڈ���eo#g ��,~ڈ���`���~ڈ��� 1�ispteam��������2����0���@ ;SQRsvy|}- �H�P�eo#g �`���eo#gO �~ڈ���eo#g(���:`���~ڈ���~ڈ�������_�a�δ�iO-\U�.C��$��e���P����eo#g+) �~ڈ���eo#g�-���,~ڈ���`���~ڈ�������u ���������������������� J�W�;2����0���eo#g�- �`���eo#g�-��� ,~ڈ���`���~ڈ�������u ���������������������� J�W�;2����0���eo#g�- �`���eo#g�n���:`���~ڈ���~ڈ���������a�δ�iO-\U�.C��$��e���P����S��^��FT��Y��h�TP�svȡ�eJÃ�V��K�C���l�n�#��[+HRZ�\�vh0QM��˩�j�������/h?vK���G ԗy�cmE�S����������xeo#g�o �~ڈ���eo#gW|���,~ڈ���`���~ڈ�������_ D���^'R��+�eo#g`| �`���eo#g�}�~ڈ���`���~ڈ���0eo#g�} �`���oo#g�w!!P:��;��~ڈ���~ڈ�����7FU��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g*�!!P:��;��~ڈ���~ڈ������XU��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g��!!P:��;��~ڈ���~ڈ�����,oU��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#ge�!!P:��;��~ڈ���~ڈ�����}U��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g��!!P:��;��~ڈ���~ڈ�����q�U��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g/�!!P:��;��~ڈ���~ڈ�����ՑU��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#gS�!!P:��;��~ڈ���~ڈ������}V��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g\� �~ڈ���oo#g��!!P:��;��~ڈ���~ڈ�����w�V��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g�!!P:��;��~ڈ���~ڈ������V��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g:!!P:��;��~ڈ���~ڈ�������V��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g�6!!P:��;��~ڈ���~ڈ������W��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#gnA!!P:��;��~ڈ���~ڈ�����W��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g�M!!P:��;��~ڈ���~ڈ�����PW��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#gB�!!P:��;��~ڈ���~ڈ�������W��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���oo#g�$ !!P:��;��~ڈ���~ڈ������W��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���|o#gd-!!P:~Kԝ�[~ڈ���~ڈ����iX��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���|o#g�C!!P:~Kԝ�[~ڈ���~ڈ����n��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���|o#g?O!!P:~Kԝ�[~ڈ���~ڈ����`z��d1ispteam����$DE *20H`lFs�-���=@��Y�3��������P���'�BC^b2/� ��P�P�P�P�P�0��������~ڈ���
there is EAPOL, association, authentication and deauthentication, can you see it?
Hi,
Sorry, I must have missed it.
The reason it is not able to connect is because the AP is configured to mixed mode security, i.e. TKIP+AES. See screenshot:
In the release note, we declare support of OPEN, WPA2 and WPA3 (not WPA mixed mode).
In the MPU side with the same chip, we did add this support so at some point I believe that it would be also added to the ThickMAC but I do not have a schedule.
Shlomi