A couple of questions:
1. Can VDD (1.8V) come up before VBAT (3.3V)?
2. Can SDIO_CLK be active before WL_EN?
Inderjit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Just to confirm: does the order in which VBAT (3.3V) and VIO (1.8) ramp up matter? Will VIO before VBAT damage the WL1271? The order is VIO before VBAT because the AM1808 requires that the 1.8V supply be up before the 3.3V supply.
Also, with PSP03.21.00.04.sdk (AM1808), SDIO clock is valid before WLAN_EN from the testing I've done. Can you confirm that this is the case?
Thanks, but it doesn't answer my question: will VIO power-up before VBAT damage the WL1271?
Hi Inderjit:
The device will not be damaged if VIO comes up before Vbat. However, before the Enable is going high, the VIO, Vbat and Slow_Clock must be present and stable.
Sincerely,
Arild