Other Parts Discussed in Thread: WL1835
Tool/software:
Dear Sirs,
We are currently using the WL1835 module on BeagleBone Black (BBB), and have followed the instructions provided in this TI E2E post regarding the new R8.9 release.
We have:
.Downloaded the firmware from the wl18xx_fw FIPS branch, which includes version 8.9.1.0.2_fips.
.Updated the driver according to the build-utilites R8.9 branch.
.Verified that both Wi-Fi and Bluetooth basic functionalities are working correctly.

However, when attempting to enter PLT mode using the calibrator tool from 18xx-ti-utils, we encounter an error and cannot proceed with production line testing.
We would like to clarify the following:
1.Is this issue caused by a mismatch between the calibrator version and the new FIPS firmware?
2.Is there an updated version of the calibrator tool that supports firmware 8.9.1.0.2_fips?
3.Is there a PLT-compatible .bin firmware image available for download or testing?
Any guidance or updated resources would be greatly appreciated.
/sywang