Part Number: CC3351MOD
Other Parts Discussed in Thread: CC3301
Hi TI Team,
We have created this new Thread for Wi-Fi (Old Thread).
We are currently performing Wi-Fi pre-compliance testing by using calibrator tool with version 1.0.0.93 on CC3351MOD TI-based Wi-Fi module, and we are facing an issue where the TX power configured using the calibrator tool.
We attempted multiple power configurations through the calibrator utility, but the measured output power during testing does not match the configured values consistently.
Test 1:
Wifi on 0dbm & 5dBm TX Power with 2.4GHz commands -->
calibrator wlan0 cc33xx_plt stop_tx
calibrator wlan0 cc33xx_plt tune_channel 1 0 0
calibrator wlan0 cc33xx_plt set_manual_calib -tx 1 -rx 1
calibrator wlan0 cc33xx_plt set_tx -default 0
calibrator wlan0 cc33xx_plt set_tx -preamble_type 1 -phy_rate 1 -tx_power 15 -gi_ltf_type 0 -pkt_mode 0 -length const packet 1500 -delay 50 -data_mode 0 -data_const_val 100 -cca 0
calibrator wlan0 cc33xx_plt start_tx
Output on Spacture Analyzer:
Test 2:
Wifi on 0dbm & 5dBm TX Power with 5GHz commands -->
calibrator wlan0 cc33xx_plt stop_tx
calibrator wlan0 cc33xx_plt tune_channel 36 1 0
calibrator wlan0 cc33xx_plt set_manual_calib -tx 1 -rx 1
calibrator wlan0 cc33xx_plt set_tx -default 0
calibrator wlan0 cc33xx_plt set_tx -preamble_type 2 -phy_rate 5 -tx_power 15 -gi_ltf_type 0 -pkt_mode 0 -length const packet 1500 -delay 50 -data_mode 0 -data_const_val 100 -cca 0
calibrator wlan0 cc33xx_plt start_tx
Output on Spacture Analyzer:
Question:
1. We are getting different wave-form on 0dBm & 5dBm power on 2.4 GHz & 5 GHz. While increasing the Tx power signal is getting distorted. Additionlly TX signal transmission is not continues, kinldy suggest the configuration for contineous transmission.
2. We are configuring this(-preamble_type 2 -phy_rate 5 -tx_power 15 -gi_ltf_type 0 -pkt_mode 0 -length const packet 1500 -delay 50 -data_mode 0 -data_const_val 100 -cca 0) parameter for Wi-Fi certification testing, is it sufficient or do we need to modify any commands, kinldy confirm or suggest the required configuration parameter for 2.4GHz and 5GHz Wi-Fi.
3. Is we need to configure CountryCode & other parameters in INI file for pre-complience testing by using CC33CONF tool?
Please let us know if any additional calibration data are required to do.
Regards,
Parv