This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are back porting wl12xx drivers from latest Compat Wireless package to my Kernel. My kernel version is 2.6.28.2. and platform is NXP LPC313X. We have interfaced WL1271 through SDIO(MMC slot 0)
I always get the "wl12xx: WARNING unsupported chip id: 0x0" error when I run the following command "ifconfig wlan0 up".
My sdio write/read operations are successful.
The log from console
mac80211 add interface type 2 mac c1f48850
sdio write 53 addr 0x1ffc4, 4 bytes
sdio write 53 addr 0x1ffc0, 4 bytes
sdio write 53 addr 0x1ffcc, 4 bytes
sdio write 53 addr 0x1ffc8, 4 bytes
sdio write 53 addr 0x1ffd4, 4 bytes
sdio write 53 addr 0x1ffd0, 4 bytes
sdio write 53 addr 0x1ffd8, 4 bytes
sdio write 52 addr 0x1fffc, byte 0x01
wl12xx: WARNING unsupported chip id: 0x0
sdio write 53 addr 0x1ffc4, 4 bytes
sdio write 53 addr 0x1ffc0, 4 bytes
sdio write 53 addr 0x1ffcc, 4 bytes
sdio write 53 addr 0x1ffc8, 4 bytes
sdio write 53 addr 0x1ffd4, 4 bytes
sdio write 53 addr 0x1ffd0, 4 bytes
sdio write 53 addr 0x1ffd8, 4 bytes
sdio write 52 addr 0x1fffc, byte 0x01
wl12xx: WARNING unsupported chip id: 0x0
sdio write 53 addr 0x1ffc4, 4 bytes
sdio write 53 addr 0x1ffc0, 4 bytes
sdio write 53 addr 0x1ffcc, 4 bytes
sdio write 53 addr 0x1ffc8, 4 bytes
sdio write 53 addr 0x1ffd4, 4 bytes
sdio write 53 addr 0x1ffd0, 4 bytes
sdio write 53 addr 0x1ffd8, 4 bytes
sdio write 52 addr 0x1fffc, byte 0x01
wl12xx: WARNING unsupported chip id: 0x0
wl12xx: ERROR firmware boot failed despite 3 retries
We have done the necessary modifications to load the all the compat wireless related KOs ( compat.ko, rfkill_backport.ko, cfg80211.ko, mac80211.ko, wl12xx.ko and wl12xx_sdio.ko)
The following modifications to sucessfully load the modules
1. Disable all SDIO power management functions in Compat wireless drivers because the our kernel doesn't support SDIO/MMC run time power management functions
2. Modified the check to "if (func->num != 0x01)" from "if (func->num != 0x02)" in wl1271_probe() functions of sdio.c(/compat-wireless-2012-02-26/drivers/net/wireless/wl12xx/sdio.c)
3. The name was modified from "wl12xx_driver" to "wl12xx" in main.c
static struct platform_driver wl12xx_driver = {
.probe = wl12xx_probe,
.remove = __devexit_p(wl12xx_remove),
#if LINUX_VERSION_CODE >= KERNEL_VERSION(2,6,30)
.id_table = wl12xx_id_table,
#endif
.driver = {
// .name = "wl12xx_driver",
.name = "wl12xx",
.owner = THIS_MODULE,
}
};\
With the above changes my wl12xx_probe() is being called successfully.
We had issues with writing to "W_ACCESS_ELP_CTRL_REG_ADDR" using "sdio_f0_writeb()" function. We used to error as (-22) EINVAL always for this register
Now we have replaced the "sdio_f0_writeb" & sdio_f0_readb" functions with "sdio_writeb" and "sdio_writeb" and "sdio_readb". now we don't see any sdio read/write failuers.
But the chip id is not being read properly and due to this firmware is not loaded.
Please let us know any suggestions on this
Thanks
Girish
Hi Girish,
lookint the kernel code it is possible to replace the "sdio_f0_writeb" & sdio_f0_readb" functions with "sdio_writeb" and "sdio_writeb" and "sdio_readb". assuming you had set the func->num to 0 in functions sdio_writeb" and "sdio_readb".
please confirm that you had done that correctly
see reference for the functions:
398 {
404 if (err_ret)
406 }
void sdio_f0_writeb(struct sdio_func *func, unsigned char b, unsigned int addr,
657 int *err_ret)
658 {
664 if (err_ret)
666 return;
667 }
670 if (err_ret)
672 }
Regards,
Eyal
Hi Eyal,
Thanks fir the reply.
I want to clarify here that I am not explicitly setting the func->num to 0 in functions sdio_writeb" and "sdio_readb". These functions are implemented in Linux-2.6.28.2/drivers/mmc/core_sdio_io.c.
I read the value of func-num as 0x1, which we guess is not correct.
I had backported the mmc stack from Linux-2.6.32 and currently I am able to use the sdio_f0_writeb and sdio_writeb functions itself.
Now the issue I am facing is the WL1271 chip id is always read as 0x0. The reason I suspect is the issue with struct sdio_func *func->num,
The Wi-FI interface in WL1271 can work with function number 0x2, however, when I load the wl12xx_sdio.ko, I get the func->num = 0x01, Which could a reason why I fail.
My system log when the mmc platform driver loaded is as follows
mmc0: card claims to support voltages below the defined range. These will be ignored.
mmc0: queuing CIS tuple 0x91 length 3
mmc0: new SDIO card at address 0001
I am new to Linux and SDIO stack. Let me the mistake I am committing here
Thanks
Girish
Hi Girish,
The logs that you got are good, it indicates that the Linux kernel had probed the SDIO and completed the negotiation with it
mmc0: card claims to support voltages below the defined range. These will be ignored.
mmc0: queuing CIS tuple 0x91 length 3
mmc0: new SDIO card at address 0001
However if you will not keep func->num to 0 then the SDIO read write transactions will not be to the right place and that could explain why the chip ID is read as 0
Regards,
Hi Girish,
Would like to touch base on the issue, were you able to have progress with that?
Regards,
Eyal
Hi Eyal,
Sorry for not replying on the progress made
We are able to make resolve the issue with reading the WL1271 chip ID. Now we are reading the chip ID as 0x4030111.
The issue is with powering-on the Bluetooth while loading the kernel. Due to this kernel was passing the function number as 0x1 and the wl12xx driver used to read/write the memory area of function 1(Bluetooth). Now after disabling the powering-on of Bluetooth and explicitly returning from wl1271_probe() for function other than 0x2, the driver will be accessing the memory are of Wi-Fi.
Still we are not sure why we should keep the BT powered-down while system booting.
We are able to load of all the Compat Wireless Modules, ifconfig wlan0 operations to assign the Mac address and starting the wlan0 interface.
With Compat Wireless -2012-02-22 and Firmware ver 03 - wl127x-fw-3.bin, and after applying the patches, we are able to get the interface up and able to connect in open mode.
http://permalink.gmane.org/gmane.linux.kernel.wireless.general/84311
http://permalink.gmane.org/gmane.linux.kernel.wireless.general/84312
However the calibration is not successful.
I am running the following command
./calibrator plt autocalibrate wlan0 /tmp/wl12xx_sdio.ko /lib/firmware/ti-connectivity/ini_files/TQS_S_2.6.ini /lib/firmware/ti-connectivity/wl1271-nvs.bin 00:01:02:03:65:29
With latest Compat wireless package (2012-04-03) and firmware ver (04 - wl127x-fw-4-sr.bin and wl127x-fw-4-plt.bin, ) I am able to successfully calibrate and nvs file sucessfully.
However, I am not able to connect to any device. there is crash in the modules. However I am able to do the scan operation successfully.
There is crash after running the following commands
ifconfig wlan0 down &
ifconfig wlan0 hw ether de:ad:be:ef:c0:fe &
iwconfig wlan0 mode ad-hoc
iwconfig wlan0 essid brady123
ifconfig wlan0 192.168.1.6 up
Please find the log below
Let us know the right version of the firmware and Compat Wireless package to be used for both calibration and successful operation
/ # dmesg
Linux version 2.6.28.2 (root@ubuntu) (gcc version 4.4.2 (GCC) ) #3 Thu Mar 22 03:04:06 PDT 2012
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: Brady BPS313XV1
Memory policy: ECC disabled, Data cache writeback
On node 0 totalpages: 8192
free_area_init_node: node 0, pgdat c024d008, node_mem_map c0262000
Normal zone: 64 pages used for memmap
Normal zone: 0 pages reserved
Normal zone: 8128 pages, LIFO batch:0
Movable zone: 0 pages used for memmap
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128
Kernel command line: console=0 rootfstype=jffs2 quiet root=/dev/mtdblock7 safefs=0 kernel=1 sku=772
irq=30 Event=0x3e bank:1 bit:30 type:0
irq=31 Event=0x54 bank:2 bit:20 type:0
irq=32 Event=0x4b bank:2 bit:11 type:0
PID hash table entries: 128 (order: 7, 512 bytes)
Console: colour dummy device 80x30
console [ttyS0] enabled
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 30012KB available (2136K code, 177K data, 88K init)
Calibrating delay loop... 89.70 BogoMIPS (lpj=448512)
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
net_namespace: 288 bytes
NET: Registered protocol family 16
cgu_init pll set at 180000000
Registering USB gadget 0x00000f20 0x02800004 (3)
LPC31: Power Management init.
NetLabel: Initializing
NetLabel: domain hash size = 128
NetLabel: protocols = UNLABELED CIPSOv4
NetLabel: unlabeled traffic allowed by default
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
NET: Registered protocol family 1
NetWinder Floating Point Emulator V0.97 (double precision)
JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
msgmni has been set to 58
alg: No test for stdrng (krng)
io scheduler noop registered (default)
Serial: 8250/16550 driver1 ports, IRQ sharing disabled
serial8250: ttyS0 at MMIO 0x15001000 (irq = 10) is a NXP16750
serial8250.0: ttyS0 at MMIO 0x15001000 (irq = 10) is a NXP16750
NAND device: Manufacturer ID: 0x20, Chip ID: 0x73 (ST Micro NAND 16MiB 3,3V 8-bit)
Bad block table found at page 32736, version 0x00
Bad block table found at page 32704, version 0x00
nand_read_bbt: Bad block at 0x00000000
nand_read_bbt: Bad block at 0x00000000
Creating 10 MTD partitions on "NAND 16MiB 3,3V 8-bit":
0x00004000-0x00018000 : "apex1"
0x00018000-0x0002c000 : "apex2"
0x0002c000-0x00030000 : "apex-env"
0x00030000-0x00050000 : "sysconfig"
0x00050000-0x00208000 : "kernel1"
0x00208000-0x003c0000 : "kernel2"
0x003c0000-0x00440000 : "configfs"
0x00440000-0x00de8000 : "rootfs"
0x00de8000-0x00fe8000 : "safefs"
0x00fe8000-0x00ff0000 : "log"
mice: PS/2 mouse device common for all mice
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog device driver initialized.
cpuidle: using governor ladder
TCP cubic registered
NET: Registered protocol family 17
ieee80211: 802.11 data/management/control stack, git-1.1.13
ieee80211: Copyright (C) 2004-2005 Intel Corporation <jketreno@linux.intel.com>
ieee80211_crypt: registered algorithm 'NULL'
ieee80211_crypt: registered algorithm 'WEP'
VFS: Mounted root (jffs2 filesystem) readonly.
Freeing init memory: 88K
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
Empty flash at 0x000021ac ends at 0x00002200
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
Freescale High-Speed USB SOC Device Controller driver (Apr 20, 2007)
g_serial gadget: Gadget Serial v2.4
g_serial gadget: g_serial ready
fsl-usb2-udc: bind to driver g_serial
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
g_serial gadget: high speed config #2: CDC ACM config
CGU: Get clock id:34 freq:6000000
CGU: Get clock id:20 freq:45000000
Powering off wl12xx<6>Powering off wl12xx<6>Powering down MMC Slot<6>Powering on wl12xx<6>lpc313x_mmc lpc313x_mmc.0: LPC313x MMC controller at irq 26
Powering up MMC Slot<4>mmc0: card claims to support voltages below the defined range. These will be ignored.
mmc0: queuing CIS tuple 0x91 length 3
mmc_attach_sdio the value of funcs=0x2
mmc_attach_sdio the value of funcs=0x2
mmc0: new SDIO card at address 0001
Powering on wl12xx<6>Compat-wireless backport release: compat-wireless-2012-04-02-2-1-g5c6c8e6
Backport based on linux-next.git next-20120403
cfg80211: Calling CRDA to update world regulatory domain
wl1271_probe: the value of func->num = 0x2
wl12xx: loaded
/ # ifconfig
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
/ #
/ # ifconfig[J -a
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
wlan0 Link encap:Ethernet HWaddr 03:00:00:00:29:00
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
/ # ifconfig wlan0 down &
onfig wlan0 hw ether de:ad:be:ef:c0:fe &
[3]+ Done ifconfig wlan0 down
/ # ifconfig wlan0 hw ether de:ad:be:ef:c0:fe &
[3]+ Done ifconfig wlan0 hw ether de:ad:be:ef:c0:fe
/ # iwconfig wlan0 mode ad-hoc
/ # iwconfig wlan0 essid brady123
/ # ifconfig wlan0 192.168.1.6 up
KERNEL[234.242778] add /devices/platform/lpc313x_mmc.0/mmc_host/mmc0/mmc0:0001/mmc0:0001:2/wl12xx/compat_firmware/wl12xx (compat_firmware)
ACTION=add
DEVPATH=/devices/platform/lpc313x_mmc.0/mmc_host/mmc0/mmc0:0001/mmc0:0001:2/wl12xx/compat_firmware/wl12xx
SUBSYSTEM=compat_firmware
FIRMWARE=ti-connectivity/wl127x-fw-4-sr.bin
ASYNC=0
SEQNUM=217
KERNEL[234.451922] remove /devices/platform/lpc313x_mmc.0/mmc_host/mmc0/mmc0:0001/mmc0:0001:2/wl12xx/compat_firmware/wl12xx (compat_firmware)
ACTION=remove
DEVPATH=/devices/platform/lpc313x_mmc.0/mmc_host/mmc0/mmc0:0001/mmc0:0001:2/wl12xx/compat_firmware/wl12xx
SUBSYSTEM=compat_firmware
FIRMWARE=ti-connectivity/wl127x-fw-4-sr.bin
ASYNC=0
SEQNUM=218
UDEV [234.464602] add /devices/platform/lpc313x_mmc.0/mmc_host/mmc0/mmc0:0001/mmc0:0001:2/wl12xx/compat_firmware/wl12xx (compat_firmware)
ACTION=add
DEVPATH=/devices/platform/lpc313x_mmc.0/mmc_host/mmc0/mmc0:0001/mmc0:0001:2/wl12xx/compat_firmware/wl12xx
SUBSYSTEM=compat_firmware
FIRMWARE=ti-connectivity/wl127x-fw-4-sr.bin
ASYNC=0
SEQNUM=217
UDEV [234.527889] remove /devices/platform/lpc313x_mmc.0/mmc_host/mmc0/mmc0:0001/mmc0:0001:2/wl12xx/compat_firmware/wl12xx (compat_firmware)
ACTION=remove
DEVPATH=/devices/platform/lpc313x_mmc.0/mmc_host/mmc0/mmc0:0001/mmc0:0001:2/wl12xx/compat_firmware/wl12xx
SUBSYSTEM=compat_firmware
FIRMWARE=ti-connectivity/wl127x-fw-4-sr.bin
ASYNC=0
SEQNUM=218
/ # dmesg
Linux version 2.6.28.2 (root@ubuntu) (gcc version 4.4.2 (GCC) ) #3 Thu Mar 22 03:04:06 PDT 2012
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: Brady BPS313XV1
Memory policy: ECC disabled, Data cache writeback
On node 0 totalpages: 8192
free_area_init_node: node 0, pgdat c024d008, node_mem_map c0262000
Normal zone: 64 pages used for memmap
Normal zone: 0 pages reserved
Normal zone: 8128 pages, LIFO batch:0
Movable zone: 0 pages used for memmap
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128
Kernel command line: console=0 rootfstype=jffs2 quiet root=/dev/mtdblock7 safefs=0 kernel=1 sku=772
irq=30 Event=0x3e bank:1 bit:30 type:0
irq=31 Event=0x54 bank:2 bit:20 type:0
irq=32 Event=0x4b bank:2 bit:11 type:0
PID hash table entries: 128 (order: 7, 512 bytes)
Console: colour dummy device 80x30
console [ttyS0] enabled
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 30012KB available (2136K code, 177K data, 88K init)
Calibrating delay loop... 89.70 BogoMIPS (lpj=448512)
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
net_namespace: 288 bytes
NET: Registered protocol family 16
cgu_init pll set at 180000000
Registering USB gadget 0x00000f20 0x02800004 (3)
LPC31: Power Management init.
NetLabel: Initializing
NetLabel: domain hash size = 128
NetLabel: protocols = UNLABELED CIPSOv4
NetLabel: unlabeled traffic allowed by default
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
NET: Registered protocol family 1
NetWinder Floating Point Emulator V0.97 (double precision)
JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
msgmni has been set to 58
alg: No test for stdrng (krng)
io scheduler noop registered (default)
Serial: 8250/16550 driver1 ports, IRQ sharing disabled
serial8250: ttyS0 at MMIO 0x15001000 (irq = 10) is a NXP16750
serial8250.0: ttyS0 at MMIO 0x15001000 (irq = 10) is a NXP16750
NAND device: Manufacturer ID: 0x20, Chip ID: 0x73 (ST Micro NAND 16MiB 3,3V 8-bit)
Bad block table found at page 32736, version 0x00
Bad block table found at page 32704, version 0x00
nand_read_bbt: Bad block at 0x00000000
nand_read_bbt: Bad block at 0x00000000
Creating 10 MTD partitions on "NAND 16MiB 3,3V 8-bit":
0x00004000-0x00018000 : "apex1"
0x00018000-0x0002c000 : "apex2"
0x0002c000-0x00030000 : "apex-env"
0x00030000-0x00050000 : "sysconfig"
0x00050000-0x00208000 : "kernel1"
0x00208000-0x003c0000 : "kernel2"
0x003c0000-0x00440000 : "configfs"
0x00440000-0x00de8000 : "rootfs"
0x00de8000-0x00fe8000 : "safefs"
0x00fe8000-0x00ff0000 : "log"
mice: PS/2 mouse device common for all mice
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog device driver initialized.
cpuidle: using governor ladder
TCP cubic registered
NET: Registered protocol family 17
ieee80211: 802.11 data/management/control stack, git-1.1.13
ieee80211: Copyright (C) 2004-2005 Intel Corporation <jketreno@linux.intel.com>
ieee80211_crypt: registered algorithm 'NULL'
ieee80211_crypt: registered algorithm 'WEP'
VFS: Mounted root (jffs2 filesystem) readonly.
Freeing init memory: 88K
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
Empty flash at 0x000021ac ends at 0x00002200
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
Freescale High-Speed USB SOC Device Controller driver (Apr 20, 2007)
g_serial gadget: Gadget Serial v2.4
g_serial gadget: g_serial ready
fsl-usb2-udc: bind to driver g_serial
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
g_serial gadget: high speed config #2: CDC ACM config
CGU: Get clock id:34 freq:6000000
CGU: Get clock id:20 freq:45000000
Powering off wl12xx<6>Powering off wl12xx<6>Powering down MMC Slot<6>Powering on wl12xx<6>lpc313x_mmc lpc313x_mmc.0: LPC313x MMC controller at irq 26
Powering up MMC Slot<4>mmc0: card claims to support voltages below the defined range. These will be ignored.
mmc0: queuing CIS tuple 0x91 length 3
mmc_attach_sdio the value of funcs=0x2
mmc_attach_sdio the value of funcs=0x2
mmc0: new SDIO card at address 0001
Powering on wl12xx<6>Compat-wireless backport release: compat-wireless-2012-04-02-2-1-g5c6c8e6
Backport based on linux-next.git next-20120403
cfg80211: Calling CRDA to update world regulatory domain
wl1271_probe: the value of func->num = 0x2
wl12xx: loaded
wl12xx: firmware booted (Rev 6.3.5.0.98)
/ # route add default gw 192.168.1.1 dev wlan0
/ # iwconfig
lo no wireless extensions.
wlan0 IEEE 802.11abgn ESSID:"brady123"
Mode:Ad-Hoc Frequency:2.412 GHz Cell: Not-Associated
Tx-Power=20 dBm
Retry long limit:7 RTS thr:off Fragment thr:off
Encryption key:off
Power Management:on
/ #
/ # iwconfig[J dmesg
wed by default
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
NET: Registered protocol family 1
NetWinder Floating Point Emulator V0.97 (double precision)
JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
msgmni has been set to 58
alg: No test for stdrng (krng)
io scheduler noop registered (default)
Serial: 8250/16550 driver1 ports, IRQ sharing disabled
serial8250: ttyS0 at MMIO 0x15001000 (irq = 10) is a NXP16750
serial8250.0: ttyS0 at MMIO 0x15001000 (irq = 10) is a NXP16750
NAND device: Manufacturer ID: 0x20, Chip ID: 0x73 (ST Micro NAND 16MiB 3,3V 8-bit)
Bad block table found at page 32736, version 0x00
Bad block table found at page 32704, version 0x00
nand_read_bbt: Bad block at 0x00000000
nand_read_bbt: Bad block at 0x00000000
Creating 10 MTD partitions on "NAND 16MiB 3,3V 8-bit":
0x00004000-0x00018000 : "apex1"
0x00018000-0x0002c000 : "apex2"
0x0002c000-0x00030000 : "apex-env"
0x00030000-0x00050000 : "sysconfig"
0x00050000-0x00208000 : "kernel1"
0x00208000-0x003c0000 : "kernel2"
0x003c0000-0x00440000 : "configfs"
0x00440000-0x00de8000 : "rootfs"
0x00de8000-0x00fe8000 : "safefs"
0x00fe8000-0x00ff0000 : "log"
mice: PS/2 mouse device common for all mice
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog device driver initialized.
cpuidle: using governor ladder
TCP cubic registered
NET: Registered protocol family 17
ieee80211: 802.11 data/management/control stack, git-1.1.13
ieee80211: Copyright (C) 2004-2005 Intel Corporation <jketreno@linux.intel.com>
ieee80211_crypt: registered algorithm 'NULL'
ieee80211_crypt: registered algorithm 'WEP'
VFS: Mounted root (jffs2 filesystem) readonly.
Freeing init memory: 88K
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
Empty flash at 0x000021ac ends at 0x00002200
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
Freescale High-Speed USB SOC Device Controller driver (Apr 20, 2007)
g_serial gadget: Gadget Serial v2.4
g_serial gadget: g_serial ready
fsl-usb2-udc: bind to driver g_serial
CGU: Get clock id:34 freq:6000000
lpc313x-wdt lpc313x-wdt: Watchdog timer closed unexpectedly
g_serial gadget: high speed config #2: CDC ACM config
CGU: Get clock id:34 freq:6000000
CGU: Get clock id:20 freq:45000000
Powering off wl12xx<6>Powering off wl12xx<6>Powering down MMC Slot<6>Powering on wl12xx<6>lpc313x_mmc lpc313x_mmc.0: LPC313x MMC controller at irq 26
Powering up MMC Slot<4>mmc0: card claims to support voltages below the defined range. These will be ignored.
mmc0: queuing CIS tuple 0x91 length 3
mmc_attach_sdio the value of funcs=0x2
mmc_attach_sdio the value of funcs=0x2
mmc0: new SDIO card at address 0001
Powering on wl12xx<6>Compat-wireless backport release: compat-wireless-2012-04-02-2-1-g5c6c8e6
Backport based on linux-next.git next-20120403
cfg80211: Calling CRDA to update world regulatory domain
wl1271_probe: the value of func->num = 0x2
wl12xx: loaded
wl12xx: firmware booted (Rev 6.3.5.0.98)
wlan0: Creating new IBSS network, BSSID c1edff10
wl12xx: ERROR command complete timeout
------------[ cut here ]------------
WARNING: at /home/bps/compat-wireless-2012-04-03/drivers/net/wireless/wl12xx/cmd.c:108 wl1271_cmd_send+0x340/0x374 [wl12xx]()
Modules linked in: wl12xx_sdio wl12xx compat_firmware_class mac80211 cfg80211 rfkill_backport compat lpc313x_mmc g_serial nxp_usb2_udc
[<c01b9990>] (dump_stack+0x0/0x14) from [<c0035cec>] (warn_on_slowpath+0x4c/0x68)
[<c0035ca0>] (warn_on_slowpath+0x0/0x68) from [<bf0b0868>] (wl1271_cmd_send+0x340/0x374 [wl12xx])
r6:c1f31970 r5:ffffff92 r4:c1f316c0
[<bf0b0528>] (wl1271_cmd_send+0x0/0x374 [wl12xx]) from [<bf0b27d0>] (wl12xx_cmd_role_start_ibss+0x140/0x180 [wl12xx])
[<bf0b2690>] (wl12xx_cmd_role_start_ibss+0x0/0x180 [wl12xx]) from [<bf0ad4c0>] (wl1271_op_bss_info_changed+0x92c/0xba4 [wl12xx])
r7:c1c36838 r6:c1c36840 r5:c1f316c0 r4:c1c368c4
[<bf0acb94>] (wl1271_op_bss_info_changed+0x0/0xba4 [wl12xx]) from [<bf064b94>] (ieee80211_bss_info_change_notify+0x170/0x184 [mac80211])
[<bf064a24>] (ieee80211_bss_info_change_notify+0x0/0x184 [mac80211]) from [<bf06ddf4>] (__ieee80211_sta_join_ibss+0x568/0x5f4 [mac80211])
r7:c1f31d74 r6:c1f50820 r5:c1e5e414 r4:c1c363e0
[<bf06d88c>] (__ieee80211_sta_join_ibss+0x0/0x5f4 [mac80211]) from [<bf06e1a0>] (ieee80211_ibss_work+0x230/0x414 [mac80211])
[<bf06df70>] (ieee80211_ibss_work+0x0/0x414 [mac80211]) from [<bf070ec0>] (ieee80211_iface_work+0x294/0x2c8 [mac80211])
[<bf070c2c>] (ieee80211_iface_work+0x0/0x2c8 [mac80211]) from [<c0045e3c>] (run_workqueue+0xbc/0x144)
[<c0045d80>] (run_workqueue+0x0/0x144) from [<c0046528>] (worker_thread+0x104/0x118)
r7:c1f5ce48 r6:c1edffa4 r5:c1ede000 r4:c1f5ce40
[<c0046424>] (worker_thread+0x0/0x118) from [<c0049b00>] (kthread+0x58/0x94)
r7:00000000 r6:c1f5ce40 r5:c0046424 r4:c1ede000
[<c0049aa8>] (kthread+0x0/0x94) from [<c0038b08>] (do_exit+0x0/0x6fc)
r7:00000000 r6:00000000 r5:00000000 r4:00000000
---[ end trace 6a06b766661523a6 ]---
wl12xx: ERROR failed to initiate cmd role enable
wl12xx: WARNING cmd join failed -110
wl12xx: ERROR command complete timeout
------------[ cut here ]------------
WARNING: at /home/bps/compat-wireless-2012-04-03/drivers/net/wireless/wl12xx/cmd.c:108 wl1271_cmd_send+0x340/0x374 [wl12xx]()
Modules linked in: wl12xx_sdio wl12xx compat_firmware_class mac80211 cfg80211 rfkill_backport compat lpc313x_mmc g_serial nxp_usb2_udc
[<c01b9990>] (dump_stack+0x0/0x14) from [<c0035cec>] (warn_on_slowpath+0x4c/0x68)
[<c0035ca0>] (warn_on_slowpath+0x0/0x68) from [<bf0b0868>] (wl1271_cmd_send+0x340/0x374 [wl12xx])
r6:c1f31970 r5:ffffff92 r4:c1f316c0
[<bf0b0528>] (wl1271_cmd_send+0x0/0x374 [wl12xx]) from [<bf0b2050>] (wl1271_cmd_configure+0x3c/0x60 [wl12xx])
[<bf0b2014>] (wl1271_cmd_configure+0x0/0x60 [wl12xx]) from [<bf0b6dcc>] (wl1271_acx_ac_cfg+0xa0/0xd4 [wl12xx])
r5:00000005 r4:c1e4cc00
[<bf0b6d2c>] (wl1271_acx_ac_cfg+0x0/0xd4 [wl12xx]) from [<bf0abac0>] (wl1271_op_conf_tx+0x90/0xfc [wl12xx])
[<bf0aba30>] (wl1271_op_conf_tx+0x0/0xfc [wl12xx]) from [<bf080208>] (ieee80211_set_wmm_default+0x19c/0x1f0 [mac80211])
[<bf08006c>] (ieee80211_set_wmm_default+0x0/0x1f0 [mac80211]) from [<bf0802d0>] (ieee80211_sta_def_wmm_params+0x74/0x78 [mac80211])
[<bf08025c>] (ieee80211_sta_def_wmm_params+0x0/0x78 [mac80211]) from [<bf06de04>] (__ieee80211_sta_join_ibss+0x578/0x5f4 [mac80211])
r5:c1e5e414 r4:c1c363e0
[<bf06d88c>] (__ieee80211_sta_join_ibss+0x0/0x5f4 [mac80211]) from [<bf06e1a0>] (ieee80211_ibss_work+0x230/0x414 [mac80211])
[<bf06df70>] (ieee80211_ibss_work+0x0/0x414 [mac80211]) from [<bf070ec0>] (ieee80211_iface_work+0x294/0x2c8 [mac80211])
[<bf070c2c>] (ieee80211_iface_work+0x0/0x2c8 [mac80211]) from [<c0045e3c>] (run_workqueue+0xbc/0x144)
[<c0045d80>] (run_workqueue+0x0/0x144) from [<c0046528>] (worker_thread+0x104/0x118)
r7:c1f5ce48 r6:c1edffa4 r5:c1ede000 r4:c1f5ce40
[<c0046424>] (worker_thread+0x0/0x118) from [<c0049b00>] (kthread+0x58/0x94)
r7:00000000 r6:c1f5ce40 r5:c0046424 r4:c1ede000
[<c0049aa8>] (kthread+0x0/0x94) from [<c0038b08>] (do_exit+0x0/0x6fc)
r7:00000000 r6:00000000 r5:00000000 r4:00000000
---[ end trace 6a06b766661523a6 ]---
wl12xx: WARNING CONFIGURE command NOK
wl12xx: WARNING acx ac cfg failed: -110
wl12xx: ERROR command complete timeout
------------[ cut here ]------------
WARNING: at /home/bps/compat-wireless-2012-04-03/drivers/net/wireless/wl12xx/cmd.c:108 wl1271_cmd_send+0x340/0x374 [wl12xx]()
Modules linked in: wl12xx_sdio wl12xx compat_firmware_class mac80211 cfg80211 rfkill_backport compat lpc313x_mmc g_serial nxp_usb2_udc
[<c01b9990>] (dump_stack+0x0/0x14) from [<c0035cec>] (warn_on_slowpath+0x4c/0x68)
[<c0035ca0>] (warn_on_slowpath+0x0/0x68) from [<bf0b0868>] (wl1271_cmd_send+0x340/0x374 [wl12xx])
r6:c1f31970 r5:ffffff92 r4:c1f316c0
[<bf0b0528>] (wl1271_cmd_send+0x0/0x374 [wl12xx]) from [<bf0b2050>] (wl1271_cmd_configure+0x3c/0x60 [wl12xx])
[<bf0b2014>] (wl1271_cmd_configure+0x0/0x60 [wl12xx]) from [<bf0b6dcc>] (wl1271_acx_ac_cfg+0xa0/0xd4 [wl12xx])
r5:0000000b r4:c1e4cc00
[<bf0b6d2c>] (wl1271_acx_ac_cfg+0x0/0xd4 [wl12xx]) from [<bf0abac0>] (wl1271_op_conf_tx+0x90/0xfc [wl12xx])
[<bf0aba30>] (wl1271_op_conf_tx+0x0/0xfc [wl12xx]) from [<bf080208>] (ieee80211_set_wmm_default+0x19c/0x1f0 [mac80211])
[<bf08006c>] (ieee80211_set_wmm_default+0x0/0x1f0 [mac80211]) from [<bf0802d0>] (ieee80211_sta_def_wmm_params+0x74/0x78 [mac80211])
[<bf08025c>] (ieee80211_sta_def_wmm_params+0x0/0x78 [mac80211]) from [<bf06de04>] (__ieee80211_sta_join_ibss+0x578/0x5f4 [mac80211])
r5:c1e5e414 r4:c1c363e0
[<bf06d88c>] (__ieee80211_sta_join_ibss+0x0/0x5f4 [mac80211]) from [<bf06e1a0>] (ieee80211_ibss_work+0x230/0x414 [mac80211])
[<bf06df70>] (ieee80211_ibss_work+0x0/0x414 [mac80211]) from [<bf070ec0>] (ieee80211_iface_work+0x294/0x2c8 [mac80211])
[<bf070c2c>] (ieee80211_iface_work+0x0/0x2c8 [mac80211]) from [<c0045e3c>] (run_workqueue+0xbc/0x144)
[<c0045d80>] (run_workqueue+0x0/0x144) from [<c0046528>] (worker_thread+0x104/0x118)
r7:c1f5ce48 r6:c1edffa4 r5:c1ede000 r4:c1f5ce40
[<c0046424>] (worker_thread+0x0/0x118) from [<c0049b00>] (kthread+0x58/0x94)
r7:00000000 r6:c1f5ce40 r5:c0046424 r4:c1ede000
[<c0049aa8>] (kthread+0x0/0x94) from [<c0038b08>] (do_exit+0x0/0x6fc)
r7:00000000 r6:00000000 r5:00000000 r4:00000000
---[ end trace 6a06b766661523a6 ]---
wl12xx: WARNING CONFIGURE command NOK
wl12xx: WARNING acx ac cfg failed: -110
wl12xx: ERROR command complete timeout
------------[ cut here ]------------
WARNING: at /home/bps/compat-wireless-2012-04-03/drivers/net/wireless/wl12xx/cmd.c:108 wl1271_cmd_send+0x340/0x374 [wl12xx]()
Modules linked in: wl12xx_sdio wl12xx compat_firmware_class mac80211 cfg80211 rfkill_backport compat lpc313x_mmc g_serial nxp_usb2_udc
[<c01b9990>] (dump_stack+0x0/0x14) from [<c0035cec>] (warn_on_slowpath+0x4c/0x68)
[<c0035ca0>] (warn_on_slowpath+0x0/0x68) from [<bf0b0868>] (wl1271_cmd_send+0x340/0x374 [wl12xx])
r6:c1f31970 r5:ffffff92 r4:c1f316c0
[<bf0b0528>] (wl1271_cmd_send+0x0/0x374 [wl12xx]) from [<bf0b2050>] (wl1271_cmd_configure+0x3c/0x60 [wl12xx])
[<bf0b2014>] (wl1271_cmd_configure+0x0/0x60 [wl12xx]) from [<bf0b6dcc>] (wl1271_acx_ac_cfg+0xa0/0xd4 [wl12xx])
r5:00000000 r4:c1e4cc00
[<bf0b6d2c>] (wl1271_acx_ac_cfg+0x0/0xd4 [wl12xx]) from [<bf0abac0>] (wl1271_op_conf_tx+0x90/0xfc [wl12xx])
[<bf0aba30>] (wl1271_op_conf_tx+0x0/0xfc [wl12xx]) from [<bf080208>] (ieee80211_set_wmm_default+0x19c/0x1f0 [mac80211])
[<bf08006c>] (ieee80211_set_wmm_default+0x0/0x1f0 [mac80211]) from [<bf0802d0>] (ieee80211_sta_def_wmm_params+0x74/0x78 [mac80211])
[<bf08025c>] (ieee80211_sta_def_wmm_params+0x0/0x78 [mac80211]) from [<bf06de04>] (__ieee80211_sta_join_ibss+0x578/0x5f4 [mac80211])
r5:c1e5e414 r4:c1c363e0
[<bf06d88c>] (__ieee80211_sta_join_ibss+0x0/0x5f4 [mac80211]) from [<bf06e1a0>] (ieee80211_ibss_work+0x230/0x414 [mac80211])
[<bf06df70>] (ieee80211_ibss_work+0x0/0x414 [mac80211]) from [<bf070ec0>] (ieee80211_iface_work+0x294/0x2c8 [mac80211])
[<bf070c2c>] (ieee80211_iface_work+0x0/0x2c8 [mac80211]) from [<c0045e3c>] (run_workqueue+0xbc/0x144)
[<c0045d80>] (run_workqueue+0x0/0x144) from [<c0046528>] (worker_thread+0x104/0x118)
r7:c1f5ce48 r6:c1edffa4 r5:c1ede000 r4:c1f5ce40
[<c0046424>] (worker_thread+0x0/0x118) from [<c0049b00>] (kthread+0x58/0x94)
r7:00000000 r6:c1f5ce40 r5:c0046424 r4:c1ede000
[<c0049aa8>] (kthread+0x0/0x94) from [<c0038b08>] (do_exit+0x0/0x6fc)
r7:00000000 r6:00000000 r5:00000000 r4:00000000
---[ end trace 6a06b766661523a6 ]---
wl12xx: WARNING CONFIGURE command NOK
wl12xx: WARNING acx ac cfg failed: -110
wl12xx: ERROR command complete timeout
------------[ cut here ]------------
WARNING: at /home/bps/compat-wireless-2012-04-03/drivers/net/wireless/wl12xx/cmd.c:108 wl1271_cmd_send+0x340/0x374 [wl12xx]()
Modules linked in: wl12xx_sdio wl12xx compat_firmware_class mac80211 cfg80211 rfkill_backport compat lpc313x_mmc g_serial nxp_usb2_udc
[<c01b9990>] (dump_stack+0x0/0x14) from [<c0035cec>] (warn_on_slowpath+0x4c/0x68)
[<c0035ca0>] (warn_on_slowpath+0x0/0x68) from [<bf0b0868>] (wl1271_cmd_send+0x340/0x374 [wl12xx])
r6:c1f31970 r5:ffffff92 r4:c1f316c0
[<bf0b0528>] (wl1271_cmd_send+0x0/0x374 [wl12xx]) from [<bf0b2050>] (wl1271_cmd_configure+0x3c/0x60 [wl12xx])
[<bf0b2014>] (wl1271_cmd_configure+0x0/0x60 [wl12xx]) from [<bf0b6dcc>] (wl1271_acx_ac_cfg+0xa0/0xd4 [wl12xx])
r5:00000000 r4:c1e4cc00
[<bf0b6d2c>] (wl1271_acx_ac_cfg+0x0/0xd4 [wl12xx]) from [<bf0abac0>] (wl1271_op_conf_tx+0x90/0xfc [wl12xx])
[<bf0aba30>] (wl1271_op_conf_tx+0x0/0xfc [wl12xx]) from [<bf080208>] (ieee80211_set_wmm_default+0x19c/0x1f0 [mac80211])
[<bf08006c>] (ieee80211_set_wmm_default+0x0/0x1f0 [mac80211]) from [<bf0802d0>] (ieee80211_sta_def_wmm_params+0x74/0x78 [mac80211])
[<bf08025c>] (ieee80211_sta_def_wmm_params+0x0/0x78 [mac80211]) from [<bf06de04>] (__ieee80211_sta_join_ibss+0x578/0x5f4 [mac80211])
r5:c1e5e414 r4:c1c363e0
[<bf06d88c>] (__ieee80211_sta_join_ibss+0x0/0x5f4 [mac80211]) from [<bf06e1a0>] (ieee80211_ibss_work+0x230/0x414 [mac80211])
[<bf06df70>] (ieee80211_ibss_work+0x0/0x414 [mac80211]) from [<bf070ec0>] (ieee80211_iface_work+0x294/0x2c8 [mac80211])
[<bf070c2c>] (ieee80211_iface_work+0x0/0x2c8 [mac80211]) from [<c0045e3c>] (run_workqueue+0xbc/0x144)
[<c0045d80>] (run_workqueue+0x0/0x144) from [<c0046528>] (worker_thread+0x104/0x118)
r7:c1f5ce48 r6:c1edffa4 r5:c1ede000 r4:c1f5ce40
[<c0046424>] (worker_thread+0x0/0x118) from [<c0049b00>] (kthread+0x58/0x94)
r7:00000000 r6:c1f5ce40 r5:c0046424 r4:c1ede000
[<c0049aa8>] (kthread+0x0/0x94) from [<c0038b08>] (do_exit+0x0/0x6fc)
r7:00000000 r6:00000000 r5:00000000 r4:00000000
---[ end trace 6a06b766661523a6 ]---
wl12xx: WARNING CONFIGURE command NOK
wl12xx: WARNING acx ac cfg failed: -110
wl12xx: Reading FW panic log
wl12xx: ERROR command complete timeout
------------[ cut here ]------------
WARNING: at /home/bps/compat-wireless-2012-04-03/drivers/net/wireless/wl12xx/cmd.c:108 wl1271_cmd_send+0x340/0x374 [wl12xx]()
Modules linked in: wl12xx_sdio wl12xx compat_firmware_class mac80211 cfg80211 rfkill_backport compat lpc313x_mmc g_serial nxp_usb2_udc
[<c01b9990>] (dump_stack+0x0/0x14) from [<c0035cec>] (warn_on_slowpath+0x4c/0x68)
[<c0035ca0>] (warn_on_slowpath+0x0/0x68) from [<bf0b0868>] (wl1271_cmd_send+0x340/0x374 [wl12xx])
r6:c1f31970 r5:ffffff92 r4:c1f316c0
[<bf0b0528>] (wl1271_cmd_send+0x0/0x374 [wl12xx]) from [<bf0b0f18>] (wl12xx_cmd_stop_fwlog+0x4c/0x7c [wl12xx])
[<bf0b0ecc>] (wl12xx_cmd_stop_fwlog+0x0/0x7c [wl12xx]) from [<bf0af38c>] (wl1271_recovery_work+0xb4/0x334 [wl12xx])
r5:c1f318ac r4:c1f316c0
[<bf0af2d8>] (wl1271_recovery_work+0x0/0x334 [wl12xx]) from [<c0045e3c>] (run_workqueue+0xbc/0x144)
[<c0045d80>] (run_workqueue+0x0/0x144) from [<c0046528>] (worker_thread+0x104/0x118)
r7:c1f5ce48 r6:c1edffa4 r5:c1ede000 r4:c1f5ce40
[<c0046424>] (worke
Hi,
From your log it looks like youare trying to work in IBSS mode.
The commands you are using (using iwconfig) are a bit obsolete (iwconfig is not fully supported any longer).
Please try the sequence as in the below link and let us know if it works better:
http://processors.wiki.ti.com/index.php/OMAP_Wireless_Connectivity_NLCP_IBSS_Configuration
Best Regards,
Eyal Reizer
"Let us know the right version of the firmware and Compat Wireless package to be used for both calibration and successful operation" +1
I asked it ~month before. But no one answered.
http://e2e.ti.com/support/low_power_rf/f/307/t/172141.aspx#634741
Hi Petrov,
Can you please explain why were your question not answered? Please get in the links you have in the e2e that you mentioned, there are build instructions for WLAN with links to the Compat that we are using and for the firmware’s that matches o that Compat.
Maybe what is confusing that as far as our Catalog offering (SDK releases) we provide Comapt and firmware that was tested by us and not the one that you get from the open source.
For example if you go to link http://processors.wiki.ti.com/index.php/OMAP_Wireless_Connectivity_OpenSource_WLAN_release_R4SP2_Engineering_Drop
You can see that the Compat is from:
And firmware is from:
git clone git://github.com/TI-OpenLink/ti-utils.git
git reset --hard d8513c2c8dfa1913e51f2b12436a4bbebc470064
Regards,
Eyal
Hi Girish,
Do you still have an issue with the IBSS?
Hi Petrov,
You are right, it is very confusing, for that reason we are releasing SDK so customers will be able to get some order in it
Regards,
Eyal
Hi Eyal,
Currently we are not trying with latest Compat Wireless package.
As the Compat Wireless-2012-02-22 (with WL1271 Firmware Rev 6.3.0.0.77) works fine for us except issue with autocalibration, we are using the same for further Wi-Fi direct verification for product.
The only issue with that version is the calibrated wl1271-nvs.bin file size is only 503 bytes instead of 912 bytes
Let you know if any issues once we try the latest Compat Wireless package
Thanks
Girish
Hi,
In case the wl1271-nvs.bin is wrong size (should be 912 bytes) then the WLAN driver will not even go up and WLAN will not work at all, so I would first like to know if you are able to bring up the WLAN, perform scan and connect to AP.
In addition the wl1271-nvs.bin is a product of the Calibration process (although there is one provided in the file system), so could you please send me the Calibration process you do and the terminal logs? (i ssume it is different than the log you provided earlier) I would like to understand if the process also the ini file that you had used.
Regards,
Eyal
Hello eyal,
I am also back porting wl12xx to my kernel (modified version of TI's linux-03.00.01.06 kernel for AM3517EVM kernel) and platform is AM3505. We have interfaced WL1271 through SDIO (MMC slot 0).
I am able to load sdio based modules of Compat Wireless package 2.6.37. With this I am able to up the wlan0 interface using ifconfig wlan0 up when PM_RUNTIME is disabled and i can scan and connect to Access Point successfully. But as i want to run calibrator utility i need to power it down, up, down and so on. So must enable PM_RUNTIME in my kernel.
Please let me know whether PM_RUNTIME is available for this kernel linux-03.00.01.0 ( which is 2.6.32 baseline kernel, if i am not wrong). And please give me direction if it is not available in this kernel. I already tried the patches given on the wireless community and i am failed to apply those patches as it seems some files should be in my kernel and which is not in my kernel.
My end goal is to run calibrator utility and hence i selected Compat wireless package 2.6.37.
Regards,
Hitesh V.
Hi Girish,
I am also back porting wl12xx to my kernel (modified version of TI's linux-03.00.01.06 kernel for AM3517EVM kernel) and platform is AM3505. We have interfaced WL1271 through SDIO (MMC slot 0).
I am able to load sdio based modules of Compat Wireless package 2.6.37. With this I am able to up the wlan0 interface using ifconfig wlan0 up when PM_RUNTIME is disabled and i can scan and connect to Access Point successfully. But as i want to run calibrator utility i need to power it down, up, down and so on. So must enable PM_RUNTIME in my kernel.
Please let me know whether PM_RUNTIME is available for this kernel linux-03.00.01.0 ( which is 2.6.32 baseline kernel, if i am not wrong). And please give me direction if it is not available in this kernel. I already tried the patches given on the wireless community and i am failed to apply those patches as it seems some files should be in my kernel and which is not in my kernel.
My end goal is to run calibrator utility and hence i selected Compat wireless package 2.6.37.
Regards,
Hitesh V.
Hi,
With PM_RUNTIME disabled have you tried doing ifconfig wlan0 down/up and made sure it is not working?
If this is the case then you may be able to write a custom power_on function and pass to mmc[1].dev->platform_data->slots[0].set_power = wl12xx_set_power.
This function would then be called when you up/down the driver and you can explicitly control the WLAN reset pin from it:
Please refer to the following link:
http://processors.wiki.ti.com/index.php/OMAP_Wireless_Connectivity_Hardware_Porting_for_new_Platform#Power_Control_.E2.80.93_without_voltage_regulator