Hi,
I am working with and AM335x evaluation module trying to get an android 4.2.2 build working with the Wilink 8. The issue I am having is that Bluetooth and Wi-Fi do not function correctly when I flash the build. When I turn on BT in settings, it turns off right away. When I turn on Wi-Fi, it takes a very long time to find networks and it loses all the networks it finds after a while. It gets stuck in connecting state.
The build I have put together attempts to the following two pages: http://processors.wiki.ti.com/index.php/WL18xx_Build_System_Scripts and http://processors.wiki.ti.com/index.php/TI-Android-JB-4.2.2-DevKit-4.1.1_DeveloperGuide#To_build_with_TI_WL18xx_support . It should be noted that instructions on the two pages on how to build for Wilink 8 differ. The exact steps I followed to produce the build are attached.
Serial and adb output of boot-up, Wifi Enable, and BT enable are attached with important sections highlighted. There is no serial output for BT enable.
If you could provide instructions on how to get a working build of Android 4.2.2 or higher for the AM335x evaluation module where BT and Wifi both function using the Wilink 8, it would be greatly appreciated.
Regards,
Beenish