I am looking into the reference design for CC3200 launchxl and have below question on the power management section
- The design is creating 3.3V output from the LDO (VCC_LDO_3V3). This 3.3V then passes through headers to create two more signals – VCC_BRD & VBAT_CC. What are the effective voltage values of the signals VCC_BRD & VBAT_CC?
- I see VBAT_CC is used to feed some input voltages of the CC3200 chip (pin 37, 39, 44, 54, 10). Can’t we instead just use the VCC_LDO_3V3 signal there? Do those pins need to have less than 3.3V?
- I assume VCC_BRD is less than 3.3V, so the boost converter (U8 ) is used to output a 3.3V signal VCC_DCDC_3V3 which is then used to flash the internal memory of the CC3200 (pin 47 –VDD_FLASH). Can’t we instead use the VCC_LDO_3V3 signal to feed to the pin 47 of CC3200?