New Uniflash version for SimpleLink CC31xx/CC32xx is available for use. The new version is 3.2.0.00023. The new version can be downloaded from http://www.ti.com/tool/uniflash.
Due to some technical issues, existing users cannot update the tool via the 'help->check for update' option so a new installation is required.
The new version offers the following enhancements:
- Service pack update: provides the ability to choose a service pack file to be downloaded to the device
- All operations can now be performed from the top menu (Format, Program, Service Pack update, Get Version, Add File)
- Recent sessions list automatically appears upon opening a configuration from the top menu or from the Recent Sessions on the opening screen
- New configuration is auto filling the Connection and Board or Device elements
- Connection and Board or Device elements have been changed to CC3x Serial(UART) Interface and SimpleLink WiFi CC3100/CC3200 respectively
- Added “unsaved*” header information when New Configuration is invoked
- Relative path support for session configuration files
The main enhancement is the Service Pack update. Please follow the ordered steps below for successful update procedure:
- Get the servicepack.bin image file from the link below.
- Format the device prior to programming. This step is essential and should be performed at least once. With next service pack updates, format operation would not be required
Note: all pre-production devices do not have the secured EFUSE burnt. In this case, the Secureoption must be explicitly indicated when format operation is applied- CC3100 devices: the device must be formatted as secured. Secure checkbox in the Format Options must be checked. Alert checkbox is optional
- CC3200 devices: the device must be formatted as unsecured. Secure and Alert checkboxes must be unchecked
- Invoke the Service Pack Update from a dedicated button or from the Operation option in the top menu
- Choose the file servicepack.bin and click OK
- Programming should begin. The version should be printed just before programming is started
The service pack installer can be found in the following link:
For further reading please refer to Uniflash User Guide. It can be found in the following link:
http://processors.wiki.ti.com/index.php/CC31xx_%26_CC32xx_UniFlash
Good luck