Hi,
I read the tutorial for Http_client demo. This is the first time i work with cloud so there is many things confuse me.
1/ I don't know where to add the code snippet in the instruction and where to place/call HTTPCli_connect function in file main.c.
I think TI should give more details for a newbie like me.
2/ Fortunately, i find this post and downloaded secure_http_client_demo.7z. Then i added file main.c into http_client demo project.
I don't know how to use this file "howmyssl.der.cer " so i do nothing with it.
I build the project and flash file. bin into CC3200.
When I run code on the board I am getting following error:
Connection to server failed. error(-102)
Error [-2011] at line [1237] in function [ConnectToHTTPServer]
Regards,
Khoa