Other Parts Discussed in Thread: WL1831
WL1831, Hands-Free Bluetooth phone esco audio data set to I2S format from G11, H11, G9, G10 pin output.
The following registers are set, but the test G11 and H11 have no signal output. Will WL1831 what register needs to be set or where the wrong settings G11 and H11 no signal output?
Send_HCI_VS_BT_IP_Set_Audio_Path 0xFD95, 0x02, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff
Wait_HCI_Command_Complete_VS_BT_IP_Set_Audio_Path_Event 5000, 0x00, 0xfd95, 0x00
Such as the red circle set 0x01 when the PCM is clock and sync output, but set 0x02 that I2S no signal output.
Send_HCI_VS_Write_CODEC_Config 0xFD06, 0x0200, 0x00, 0x00001f40, 0x0000, 0x01, 0x01, 0x00, 0x0010, 0x0001, 0x01, 0x0010, 0x0001, 0x00, 0x00, 0x0010, 0x0011, 0x00, 0x0010, 0x0011, 0x01, 0x00
Wait_HCI_Command_Complete_VS_Write_CODEC_Config_Event 5000, 0x00, 0xfd06, 0x00
Send_HCI_VS_Write_CODEC_Config_Enhanced 0xFD07, 0x00, 0x0000, 0x0000, 0x00, 0x04, 0x04, 0x01, 0x00, 0x00000000, 0x00, 0x00, 0x04, 0x04, 0x01, 0x00, 0x00000000, 0x00, 0x00
Wait_HCI_Command_Complete_VS_Write_CODEC_Config_Enhanced_Event 5000, 0x00, 0xfd07, 0x00