This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi, I am trying to work with BT of wl1835 on linux 3.12
With the help of TI Guide ,the basic BT function is OK,
I start SS1BTPM& LinuxSPPM
two BT devices can find each other ,can connect together and send/receive data successfully
But the BT communication distance is too short (about less than 40cm, RSSI about -60~-80dB).
when the distance of two BT devices become more than 100cm , RSSI drop to -96~-100dB,and
can not communicate successfully.
the wifi module works well , wifi and BT use the same antenna.
Below is my custom board info:
1. custom am437x_evm board with SDK AM437xSDK 07_01_00_00
2. TI Bluetooth Stack --AM335xBluetopiaLinuxProduction-4.2.1.0.1.0
3. TI bt service package --wl18xx_bt_sp_v4.2
So, Is there any suggestion or solution to this problem ?
Thanks!