Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: UNIFLASH, CC3220SF, CC3220S
Hi community !
I have read all the other threads on "sl_Start hangs" and they did not help.
It has been quite hard to chase that one down because I was not able to reproduce with a very simple code. Here below the simplest version of my code that still represents what I want to achieve:
void wifi_process(void) {
switch(state) {
case 2:
sl_Start(0, 0, 0);
break;
case 20:
sl_WlanSetMode(ROLE_AP);
break;
case 21:
sl_Stop(0);
sl_Start(0, 0, 0);
DEBUG_INFO("Success! :)\r\n");
break;
case 22:
return;
default:
break;
}
++state;
}
The 2nd call to sl_Start hangs for about 1min and then throw a "[ERROR] - FATAL ERROR: Async event timeout detected [event opcode =0x8]".
It must be a kind of timing issue, because when having a lot of debug output (on the UART ), the issue is NOT present, when removing debug output, the issue appears...
Another way to "toggle" the issue (present / not present) is to add (enough) other processes in the forever loop! Note that if only the wifi_process() function above is present in the forever loop, everything is fine...
Now, an even more funny thing is (which I hope can give you, experts out there, a clue) : while the issue was happening consistently using the debugger, I simply loaded another program (demo example from SDK 1.6) to the chip with UniFlash. Then, WITHOUT changing anything to my code, run the debugger again, and the issue was gone !!! This does not make any sense to me, and I truly hope someone can shine some light on this issue.
Thanks a bunch !
Note that all this happens while using the debugging functionality in CCS v7.3.
SDK 1.60.0.04
Below, more code to illustrate the weirdness of the problem...
NOT working:
// Forever Loop
for(;;) {
/* The SimpleLink host driver architecture mandate calling 'sl_task' in a NO-RTOS application's main loop. */
/* The purpose of this call, is to handle asynchronous events and get flow control information sent from the NWP.*/
/* Every event is classified and later handled by the host driver event handlers. */
sl_Task(NULL);
/* Modules process functions */
wifi_process();
other_process_A();
other_process_B();
other_process_C();
other_process_D();
other_process_E();
other_process_F();
other_process_G();
other_process_H();
other_process_I();
other_process_J();
other_process_K();
other_process_L();
}
Working !
// Forever Loop
for(;;) {
/* The SimpleLink host driver architecture mandate calling 'sl_task' in a NO-RTOS application's main loop. */
/* The purpose of this call, is to handle asynchronous events and get flow control information sent from the NWP.*/
/* Every event is classified and later handled by the host driver event handlers. */
sl_Task(NULL);
/* Modules process functions */
wifi_process();
// other_process_A();
// other_process_B();
// other_process_C();
// other_process_D();
// other_process_E();
// other_process_F();
// other_process_G();
// other_process_H();
// other_process_I();
// other_process_J();
// other_process_K();
// other_process_L();
}